This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 需求解决方案5V/10W

Guru**** 2867080 points

Other Parts Discussed in Thread: UCC28600, UCC28740

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1256784/requirement-solutions-5v-10w

主题中讨论的其他器件:PMP8851UCC28740、UCC28600
尊敬的先生:
根据以下要求、我需要一个解决方案。 我给出了两个输入范围。 当我需要解决方案1要求时、我可以根据设计组装元件、  我需要解决方案2要求、我可以根据设计组装元件。
方案1. 输入电压-80VAC 至264VAC/ 75VDC 至400VDC
        输出电压- 5V/2A
方案2. 输入电压- 15VDC 至60VDC
        输出电压- 5V/2A
保护:输入欠压/过压、过载、短路、输出过压和过热。
线路和负载调节-1%