Other Parts Discussed in Thread: BQ25628
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ256281、电池电压:4.1V;
220mA 45;
3、输出电流: 0.1mA -100mA
4、电池化学:锂离子;
5、电池充电电流:100mA;
充电效率对于我们的设计来说非常重要,充电芯片被用在无线电源传输系统中,用作接收器和电池充电器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.