This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] UCC28070:初始动态/瞬态负载/脉冲负载响应

Guru**** 2538950 points
Other Parts Discussed in Thread: UCC28070

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1243119/ucc28070-initial-dynamic-transient-load-pulse-load-response

器件型号:UCC28070

您好!  

我正在寻找利用 UCC28070优化 PFC 电路/升压转换器响应的技术指南。 我们有一个采用3相208V 交流输入和350Vdc 输出以及6KW 连续负载的设计。

我可以在350Vdc 调节的静态负载下消耗全功率、但 在初始动态负载或50mSec 脉冲负载下瞬态负载0A 到5A 时使350Vdc 输出下降到330Vdc。 UCC28070是否能够响应此类瞬态负载?