This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 电池保护和放大器;适用于 LiMnO2的电量监测计选择

Guru**** 2575725 points
Other Parts Discussed in Thread: BQ77905, BQ77915, BQ34Z100-R2, BQ2052, BQ35100

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1236177/battery-protection-fuel-gauge-selection-for-limno2

主题中讨论的其他器件:BQ34Z100-R2、BQ77905 、BQ77915 BQ2052、BQ35100

您好!

需要适用于 LiMnO2电池组的电池保护和电量监测计选择支持

1.电池组配置5S2P
2.电池组电压15V/SW 3100mA

电池特性
 标称容量(100欧姆接通、2V 切断) 1550 mA
 典型电压(在+ 20 °C 下):3.2V 至3.3V  
 标准连续放电电流20 mA
 最大持续放电电流60 mA
 最大异常充电电流25 mA
 标称能量4.65Wh
 交流阻抗@ 1kHz 250m Ω

此致、