This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ76952:使用 STM32F103微控制器进行 BQ76952 I2C 编程存在问题!

Guru**** 2811575 points

Other Parts Discussed in Thread: BQ76952

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1239948/bq76952-bq76952-i2c-programming-with-stm32f103-microcontroller-issue

器件型号:BQ76952

您好,先生,我有 BQ76952 IC ,我想读我的 BMS 的温度和电芯电压和 I2C 的写操作, 我尝试相同的不同代码,但两个通信没有稳定,我还连接示波器检查时钟和数据,但没有任何类型的脉冲/时钟我在这里看到. 和通过相同的 I2C 程序(只是我已经更改设备添加并尝试与其他通信(例如 MPU6050)。连接是稳定的,

我正在等待重放...

谢谢。此

致、
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    您知道所使用的器件是否支持时钟延展? 如果同一个程序在另一个 MCU 上运行、则意味着不工作的 MCU 的硬件不足或器件配置不正确。 一个问题可能是其中一个 MCU 上的 I2C 通信时钟未正确配置。 您在每个器件上设置的配置是否有差异?

    此致!

    A·内德尔费尔德

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您快速重播、  

    " 我知道,我不会骗你的。" 但我无法读取正确的数据(例如、 特定温度下) 进行的。 可以获取 STM32的示例代码以读取温度传感器。

    如果有、请附上。

    我用于通过 UART 获取 BQ79XXX 数据。 并得到这一信息?/

    1304.349976温度1
    1304.349976温度1
    1304.349976温度1
    1304.349976温度1
    1304.349976温度1
    1304.349976温度1
    1304.349976温度1
    1304.349976温度1
    1304.349976温度1
    1304.349976温度1

    先生我被用在下面的代码...

    ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2021, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*//* USER CODE BEGIN Header */
    /**
      ******************************************************************************
      * @file           : main.c
      * @brief          : Main program body 
      * (Non-USER sections generated from STM32CubeMX software)
      ******************************************************************************
      * @attention
      *
      * <h2><center>Copyright Copyright (c) 2020 STMicroelectronics.
      * All rights reserved.</center></h2>
      *
      * This software component is licensed by ST under BSD 3-Clause license,
      * the "License"; You may not use this file except in compliance with the
      * License. You may obtain a copy of the License at:
      *                        opensource.org/licenses/BSD-3-Clause
      *
      ******************************************************************************
      */
    //  BQ76952EVM demo code for STM32 NUCLEO-F103RB + BQ76952EVM 
    //
    //  Connection description: The I2C SCL and SDA pins are the only pin connections required between the
    //  NUCLEO board and the BQ76952EVM for this demo code. Also a ground connection should be made between the 2 boards.
    //  The ALERT, RST_SHUT, and DFETOFF pins are also configured on the MCU and can be used as shown.
    //
    //                                     /|\ /|\ 
    //                   STM32             5k |
    //                 -----------------    |  5k
    //                |             PB8 |---+---|-- I2C Clock (SCL)
    //                |                 |       |
    //                |		PB9 |-------+-- I2C Data (SDA)
    //                |                 |
    //     DFETOFF ---| PA8             |
    //                |                 |
    //   RST_SHUT  ---| PA9             |--- Green LED
    //                |                 |
    //      ALERT  ---|PA10             |
    //                |                 |
    
    
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    #include <stdio.h>
    #include "BQ769x2Header.h"
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    #define DEV_ADDR  0x10  // BQ769x2 address is 0x10 including R/W bit or 0x8 as 7-bit address
    #define CRC_Mode 0  // 0 for disabled, 1 for enabled
    #define MAX_BUFFER_SIZE 10
    #define R 0 // Read; Used in DirectCommands and Subcommands functions
    #define W 1 // Write; Used in DirectCommands and Subcommands functions
    #define W2 2 // Write data with two bytes; Used in Subcommands function
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    I2C_HandleTypeDef hi2c1;
    
    TIM_HandleTypeDef htim1;
    
    UART_HandleTypeDef huart2;
    
    /* USER CODE BEGIN PV */
    uint8_t RX_data [2] = {0x00, 0x00}; // used in several functions to store data read from BQ769x2
    uint8_t RX_32Byte [32] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 
    	0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    	//used in Subcommands read function
    // Global Variables for cell voltages, temperatures, Stack voltage, PACK Pin voltage, LD Pin voltage, CC2 current
    uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    float Temperature [3] = {0,0,0};
    uint16_t Stack_Voltage = 0x00;
    uint16_t Pack_Voltage = 0x00;
    uint16_t LD_Voltage = 0x00;
    uint16_t Pack_Current = 0x00;
    
    uint16_t AlarmBits = 0x00;
    uint8_t value_SafetyStatusA;  // Safety Status Register A
    uint8_t value_SafetyStatusB;  // Safety Status Register B
    uint8_t value_SafetyStatusC;  // Safety Status Register C
    uint8_t value_PFStatusA;   // Permanent Fail Status Register A
    uint8_t value_PFStatusB;   // Permanent Fail Status Register B
    uint8_t value_PFStatusC;   // Permanent Fail Status Register C
    uint8_t FET_Status;  // FET Status register contents  - Shows states of FETs
    uint16_t CB_ActiveCells;  // Cell Balancing Active Cells
    
    uint8_t	UV_Fault = 0;   // under-voltage fault state
    uint8_t	OV_Fault = 0;   // over-voltage fault state
    uint8_t	SCD_Fault = 0;  // short-circuit fault state
    uint8_t	OCD_Fault = 0;  // over-current fault state
    uint8_t ProtectionsTriggered = 0; // Set to 1 if any protection triggers
    
    uint8_t LD_ON = 0;	// Load Detect status bit
    uint8_t DSG = 0;   // discharge FET state
    uint8_t CHG = 0;   // charge FET state
    uint8_t PCHG = 0;  // pre-charge FET state
    uint8_t PDSG = 0;  // pre-discharge FET state
    
    uint32_t AccumulatedCharge_Int; // in BQ769x2_READPASSQ func
    uint32_t AccumulatedCharge_Frac;// in BQ769x2_READPASSQ func
    uint32_t AccumulatedCharge_Time;// in BQ769x2_READPASSQ func
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_I2C1_Init(void);
    static void MX_USART2_UART_Init(void);
    static void MX_TIM1_Init(void);
    /* USER CODE BEGIN PFP */
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    void delayUS(uint32_t us) {   // Sets the delay in microseconds.
    	__HAL_TIM_SET_COUNTER(&htim1,0);  // set the counter value a 0
    	while (__HAL_TIM_GET_COUNTER(&htim1) < us);  // wait for the counter to reach the us input in the parameter
    }
    
    void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
    {
        uint8_t copyIndex = 0;
        for (copyIndex = 0; copyIndex < count; copyIndex++)
        {
            dest[copyIndex] = source[copyIndex];
        }
    }
    
    unsigned char Checksum(unsigned char *ptr, unsigned char len)
    // Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.	
    {
    	unsigned char i;
    	unsigned char checksum = 0;
    
    	for(i=0; i<len; i++)
    		checksum += ptr[i];
    
    	checksum = 0xff & ~checksum;
    
    	return(checksum);
    }
    
    unsigned char CRC8(unsigned char *ptr, unsigned char len)
    //Calculates CRC8 for passed bytes. Used in i2c read and write functions 
    {
    	unsigned char i;
    	unsigned char crc=0;
    	while(len--!=0)
    	{
    		for(i=0x80; i!=0; i/=2)
    		{
    			if((crc & 0x80) != 0)
    			{
    				crc *= 2;
    				crc ^= 0x107;
    			}
    			else
    				crc *= 2;
    
    			if((*ptr & i)!=0)
    				crc ^= 0x107;
    		}
    		ptr++;
    	}
    	return(crc);
    }
    
    void I2C_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
    	uint8_t TX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    #if CRC_Mode
    	{
    		uint8_t crc_count = 0;
    		crc_count = count * 2;
    		uint8_t crc1stByteBuffer [3] = {0x10, reg_addr, reg_data[0]};
    		unsigned int j;
    		unsigned int i;
    		uint8_t temp_crc_buffer [3];
    
    		TX_Buffer[0] = reg_data[0];
    		TX_Buffer[1] = CRC8(crc1stByteBuffer,3);
    
    		j = 2;
    		for(i=1; i<count; i++)
    		{
    			TX_Buffer[j] = reg_data[i];
    			j = j + 1;
    			temp_crc_buffer[0] = reg_data[i];
    			TX_Buffer[j] = CRC8(temp_crc_buffer,1);
    			j = j + 1;
    		}
    		HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, TX_Buffer, crc_count, 1000);
    	}
    #else 
    	HAL_I2C_Mem_Write(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
    #endif
    }
    
    int I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
    {
    	unsigned int RX_CRC_Fail = 0;  // reset to 0. If in CRC Mode and CRC fails, this will be incremented.
    	uint8_t RX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    #if CRC_Mode
    	{
    		uint8_t crc_count = 0;
    		uint8_t ReceiveBuffer [10] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
    		crc_count = count * 2;
    		unsigned int j;
    		unsigned int i;
    		unsigned char CRCc = 0;
    		uint8_t temp_crc_buffer [3];
    
    		HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, ReceiveBuffer, crc_count, 1000);
    		uint8_t crc1stByteBuffer [4] = {0x10, reg_addr, 0x11, ReceiveBuffer[0]};
    		CRCc = CRC8(crc1stByteBuffer,4);
    		if (CRCc != ReceiveBuffer[1])
    		{
    			RX_CRC_Fail += 1;
    		}
    		RX_Buffer[0] = ReceiveBuffer[0];
    
    		j = 2;
    		for (i=1; i<count; i++)
    		{
    			RX_Buffer[i] = ReceiveBuffer[j];
    			temp_crc_buffer[0] = ReceiveBuffer[j];
    			j = j + 1;
    			CRCc = CRC8(temp_crc_buffer,1);
    			if (CRCc != ReceiveBuffer[j])
    				RX_CRC_Fail += 1;
    			j = j + 1;
    		}
    		CopyArray(RX_Buffer, reg_data, crc_count);
    	}
    #else
    	HAL_I2C_Mem_Read(&hi2c1, DEV_ADDR, reg_addr, 1, reg_data, count, 1000);
    #endif
    	return 0;
    }
    
    void BQ769x2_SetRegister(uint16_t reg_addr, uint32_t reg_data, uint8_t datalen)
    {
    	uint8_t TX_Buffer[2] = {0x00, 0x00};
    	uint8_t TX_RegData[6] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
    
    	//TX_RegData in little endian format
    	TX_RegData[0] = reg_addr & 0xff; 
    	TX_RegData[1] = (reg_addr >> 8) & 0xff;
    	TX_RegData[2] = reg_data & 0xff; //1st byte of data
    
    	switch(datalen)
        {
    		case 1: //1 byte datalength
          		I2C_WriteReg(0x3E, TX_RegData, 3);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 3); 
    			TX_Buffer[1] = 0x05; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
    		case 2: //2 byte datalength
    			TX_RegData[3] = (reg_data >> 8) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData, 4);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 4); 
    			TX_Buffer[1] = 0x06; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
    		case 4: //4 byte datalength, Only used for CCGain and Capacity Gain
    			TX_RegData[3] = (reg_data >> 8) & 0xff;
    			TX_RegData[4] = (reg_data >> 16) & 0xff;
    			TX_RegData[5] = (reg_data >> 24) & 0xff;
    			I2C_WriteReg(0x3E, TX_RegData, 6);
    			delayUS(2000);
    			TX_Buffer[0] = Checksum(TX_RegData, 6); 
    			TX_Buffer[1] = 0x08; //combined length of register address and data
          		I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length
    			delayUS(2000);
    			break;
        }
    }
    
    void CommandSubcommands(uint16_t command) //For Command only Subcommands
    // See the TRM or the BQ76952 header file for a full list of Command-only subcommands
    {	//For DEEPSLEEP/SHUTDOWN subcommand you will need to call this function twice consecutively
    	
    	uint8_t TX_Reg[2] = {0x00, 0x00};
    
    	//TX_Reg in little endian format
    	TX_Reg[0] = command & 0xff;
    	TX_Reg[1] = (command >> 8) & 0xff;
    
    	I2C_WriteReg(0x3E,TX_Reg,2); 
    	delayUS(2000);
    }
    
    void Subcommands(uint16_t command, uint16_t data, uint8_t type)
    // See the TRM or the BQ76952 header file for a full list of Subcommands
    {
    	//security keys and Manu_data writes dont work with this function (reading these commands works)
    	//max readback size is 32 bytes i.e. DASTATUS, CUV/COV snapshot
    	uint8_t TX_Reg[4] = {0x00, 0x00, 0x00, 0x00};
    	uint8_t TX_Buffer[2] = {0x00, 0x00};
    
    	//TX_Reg in little endian format
    	TX_Reg[0] = command & 0xff;
    	TX_Reg[1] = (command >> 8) & 0xff; 
    
    	if (type == R) {//read
    		I2C_WriteReg(0x3E,TX_Reg,2);
    		delayUS(2000);
    		I2C_ReadReg(0x40, RX_32Byte, 32); //RX_32Byte is a global variable
    	}
    	else if (type == W) {
    		//FET_Control, REG12_Control
    		TX_Reg[2] = data & 0xff; 
    		I2C_WriteReg(0x3E,TX_Reg,3);
    		delayUS(1000);
    		TX_Buffer[0] = Checksum(TX_Reg, 3);
    		TX_Buffer[1] = 0x05; //combined length of registers address and data
    		I2C_WriteReg(0x60, TX_Buffer, 2);
    		delayUS(1000); 
    	}
    	else if (type == W2){ //write data with 2 bytes
    		//CB_Active_Cells, CB_SET_LVL
    		TX_Reg[2] = data & 0xff; 
    		TX_Reg[3] = (data >> 8) & 0xff;
    		I2C_WriteReg(0x3E,TX_Reg,4);
    		delayUS(1000);
    		TX_Buffer[0] = Checksum(TX_Reg, 4); 
    		TX_Buffer[1] = 0x06; //combined length of registers address and data
    		I2C_WriteReg(0x60, TX_Buffer, 2);
    		delayUS(1000); 
    	}
    }
    
    void DirectCommands(uint8_t command, uint16_t data, uint8_t type)
    // See the TRM or the BQ76952 header file for a full list of Direct Commands
    {	//type: R = read, W = write
    	uint8_t TX_data[2] = {0x00, 0x00};
    
    	//little endian format
    	TX_data[0] = data & 0xff;
    	TX_data[1] = (data >> 8) & 0xff;
    
    	if (type == R) {//Read
    		I2C_ReadReg(command, RX_data, 2); //RX_data is a global variable
    		delayUS(2000);
    	}
    	if (type == W) {//write
        //Control_status, alarm_status, alarm_enable all 2 bytes long
    		I2C_WriteReg(command,TX_data,2);
    		delayUS(2000);
    	}
    }
    
    void BQ769x2_Init() {
    	// Configures all parameters in device RAM
    
    	// Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings
    	// See TRM for full description of CONFIG_UPDATE mode
    	CommandSubcommands(SET_CFGUPDATE);
    
    	// After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be
    	// programmed for the change to take effect. All of the RAM registers are described in detail in the BQ769x2 TRM.
    	// An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name,
    	// a full description of the register and the bits will pop up on the screen.
    
    	// 'Power Config' - 0x9234 = 0x2D80
    	// Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode
      	// Set wake speed bits to 00 for best performance
    	BQ769x2_SetRegister(PowerConfig, 0x2D80, 2);
    
    	// 'REG0 Config' - set REG0_EN bit to enable pre-regulator
    	BQ769x2_SetRegister(REG0Config, 0x01, 1);
    
    	// 'REG12 Config' - Enable REG1 with 3.3V output (0x0D for 3.3V, 0x0F for 5V)
    	BQ769x2_SetRegister(REG12Config, 0x0D, 1);
    
    	// Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable)
    	BQ769x2_SetRegister(DFETOFFPinConfig, 0x42, 1);
    
    	// Set up ALERT Pin - 0x92FC = 0x2A
    	// This configures the ALERT pin to drive high (REG1 voltage) when enabled.
    	// The ALERT pin can be used as an interrupt to the MCU when a protection has triggered or new measurements are available
    	BQ769x2_SetRegister(ALERTPinConfig, 0x2A, 1);
    
    	// Set TS1 to measure Cell Temperature - 0x92FD = 0x07
    	BQ769x2_SetRegister(TS1Config, 0x07, 1);
    
    	// Set TS3 to measure FET Temperature - 0x92FF = 0x0F
    	BQ769x2_SetRegister(TS3Config, 0x0F, 1);
    
    	// Set HDQ to measure Cell Temperature - 0x9300 = 0x07
    	BQ769x2_SetRegister(HDQPinConfig, 0x00, 1);  // No thermistor installed on EVM HDQ pin, so set to 0x00
    
    	// 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000; Writing 0x0000 sets the default of 16 cells
    	BQ769x2_SetRegister(VCellMode, 0x0000, 2);
    
    	// Enable protections in 'Enabled Protections A' 0x9261 = 0xBC
    	// Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge),
    	// COV (over-voltage), CUV (under-voltage)
    	BQ769x2_SetRegister(EnabledProtectionsA, 0xBC, 1);
    
    	// Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7
    	// Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge),
    	// OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge)
    	BQ769x2_SetRegister(EnabledProtectionsB, 0xF7, 1);
    
    	// 'Default Alarm Mask' - 0x..82 Enables the FullScan and ADScan bits, default value = 0xF800
    	BQ769x2_SetRegister(DefaultAlarmMask, 0xF882, 2);
    
    	// Set up Cell Balancing Configuration - 0x9335 = 0x03   -  Automated balancing while in Relax or Charge modes
    	// Also see "Cell Balancing with BQ769x2 Battery Monitors" document on ti.com
    	BQ769x2_SetRegister(BalancingConfiguration, 0x03, 1);
    
    	// Set up CUV (under-voltage) Threshold - 0x9275 = 0x31 (2479 mV)
    	// CUV Threshold is this value multiplied by 50.6mV
    	BQ769x2_SetRegister(CUVThreshold, 0x31, 1);
    
    	// Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV)
    	// COV Threshold is this value multiplied by 50.6mV
    	BQ769x2_SetRegister(COVThreshold, 0x55, 1);
    
    	// Set up OCC (over-current in charge) Threshold - 0x9280 = 0x05 (10 mV = 10A across 1mOhm sense resistor) Units in 2mV
    	BQ769x2_SetRegister(OCCThreshold, 0x05, 1);
    
    	// Set up OCD1 Threshold - 0x9282 = 0x0A (20 mV = 20A across 1mOhm sense resistor) units of 2mV
    	BQ769x2_SetRegister(OCD1Threshold, 0x0A, 1);
    
    	// Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor)  0x05=100mV
    	BQ769x2_SetRegister(SCDThreshold, 0x05, 1);
    
    	// Set up SCD Delay - 0x9287 = 0x03 (30 us) Enabled with a delay of (value - 1) * 15 µs; min value of 1    
    	BQ769x2_SetRegister(SCDDelay, 0x03, 1);
    
    	// Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01
    	// If this is not set, then SCD will recover based on time (SCD Recovery Time parameter).
    	BQ769x2_SetRegister(SCDLLatchLimit, 0x01, 1);
    
    	// Exit CONFIGUPDATE mode  - Subcommand 0x0092
    	CommandSubcommands(EXIT_CFGUPDATE);
    }
    
    
    
    
    
    
    
    
    
    
    
    //  ********************************* FET Control Commands  ***************************************
    
    void BQ769x2_BOTHOFF () {
    	// Disables all FETs using the DFETOFF (BOTHOFF) pin
    	// The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);  // DFETOFF pin (BOTHOFF) set high
    }
    
    void BQ769x2_RESET_BOTHOFF () {
    	// Resets DFETOFF (BOTHOFF) pin
    	// The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
    }
    
    void BQ769x2_ReadFETStatus() { 
    	// Read FET Status to see which FETs are enabled
    	DirectCommands(FETStatus, 0x00, R);
    	FET_Status = (RX_data[1]*256 + RX_data[0]);
    	DSG = ((0x4 & RX_data[0])>>2);// discharge FET state
      	CHG = (0x1 & RX_data[0]);// charge FET state
      	PCHG = ((0x2 & RX_data[0])>>1);// pre-charge FET state
      	PDSG = ((0x8 & RX_data[0])>>3);// pre-discharge FET state
    }
    
    // ********************************* End of FET Control Commands *********************************
    
    // ********************************* BQ769x2 Power Commands   *****************************************
    
    void BQ769x2_ShutdownPin() {
    	// Puts the device into SHUTDOWN mode using the RST_SHUT pin
    	// The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function	
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);  // Sets RST_SHUT pin
    }
    
    void BQ769x2_ReleaseShutdownPin() {
    	// Releases the RST_SHUT pin
    	// The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function	
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // Resets RST_SHUT pin
    }
    
    // ********************************* End of BQ769x2 Power Commands   *****************************************
    
    
    // ********************************* BQ769x2 Status and Fault Commands   *****************************************
    
    uint16_t BQ769x2_ReadAlarmStatus() { 
    	// Read this register to find out why the ALERT pin was asserted
    	DirectCommands(AlarmStatus, 0x00, R);
    	return (RX_data[1]*256 + RX_data[0]);
    }
    
    void BQ769x2_ReadSafetyStatus() { //good example functions
    	// Read Safety Status A/B/C and find which bits are set
    	// This shows which primary protections have been triggered
    	DirectCommands(SafetyStatusA, 0x00, R);
    	value_SafetyStatusA = (RX_data[1]*256 + RX_data[0]);
    	//Example Fault Flags
    	UV_Fault = ((0x4 & RX_data[0])>>2); 
    	OV_Fault = ((0x8 & RX_data[0])>>3);
    	SCD_Fault = ((0x8 & RX_data[1])>>3);
    	OCD_Fault = ((0x2 & RX_data[1])>>1);
    	DirectCommands(SafetyStatusB, 0x00, R);
    	value_SafetyStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(SafetyStatusC, 0x00, R);
    	value_SafetyStatusC = (RX_data[1]*256 + RX_data[0]);
    	if ((value_SafetyStatusA + value_SafetyStatusB + value_SafetyStatusC) > 1) {
    		ProtectionsTriggered = 1; }
    	else {
    		ProtectionsTriggered = 0; }
    }
    
    void BQ769x2_ReadPFStatus() {
    	// Read Permanent Fail Status A/B/C and find which bits are set
    	// This shows which permanent failures have been triggered
    	DirectCommands(PFStatusA, 0x00, R);
    	value_PFStatusA = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(PFStatusB, 0x00, R);
    	value_PFStatusB = (RX_data[1]*256 + RX_data[0]);
    	DirectCommands(PFStatusC, 0x00, R);
    	value_PFStatusC = (RX_data[1]*256 + RX_data[0]);
    }
    
    // ********************************* End of BQ769x2 Status and Fault Commands   *****************************************
    
    
    // ********************************* BQ769x2 Measurement Commands   *****************************************
    
    
    uint16_t BQ769x2_ReadVoltage(uint8_t command)
    // This function can be used to read a specific cell voltage or stack / pack / LD voltage
    {
    	//RX_data is global var
    	DirectCommands(command, 0x00, R);
    	if(command >= Cell1Voltage && command <= Cell16Voltage) {//Cells 1 through 16 (0x14 to 0x32)
    		return (RX_data[1]*256 + RX_data[0]); //voltage is reported in mV
    	}
    	else {//stack, Pack, LD
    		return 10 * (RX_data[1]*256 + RX_data[0]); //voltage is reported in 0.01V units
    	}
    
    }
    void BQ769x2_ReadAllVoltages()
    // Reads all cell voltages, Stack voltage, PACK pin voltage, and LD pin voltage
    {
      int cellvoltageholder = Cell1Voltage; //Cell1Voltage is 0x14
      for (int x = 0; x < 16; x++){//Reads all cell voltages
        CellVoltage[x] = BQ769x2_ReadVoltage(cellvoltageholder);
        cellvoltageholder = cellvoltageholder + 2;
      }
      Stack_Voltage = BQ769x2_ReadVoltage(StackVoltage);
      Pack_Voltage = BQ769x2_ReadVoltage(PACKPinVoltage);
      LD_Voltage = BQ769x2_ReadVoltage(LDPinVoltage);
    }
    
    uint16_t BQ769x2_ReadCurrent() 
    // Reads PACK current 
    {
    	DirectCommands(CC2Current, 0x00, R);
    	return (RX_data[1]*256 + RX_data[0]);  // current is reported in mA
    }
    
    float BQ769x2_ReadTemperature(uint8_t command) 
    {
    	DirectCommands(command, 0x00, R);
    	//RX_data is a global var
    	return (0.1 * (float)(RX_data[1]*256 + RX_data[0])) - 273.15;  // converts from 0.1K to Celcius
    }
    
    void BQ769x2_ReadPassQ(){ // Read Accumulated Charge and Time from DASTATUS6 
    	Subcommands(DASTATUS6, 0x00, R);
    	AccumulatedCharge_Int = ((RX_32Byte[3]<<24) + (RX_32Byte[2]<<16) + (RX_32Byte[1]<<8) + RX_32Byte[0]); //Bytes 0-3
    	AccumulatedCharge_Frac = ((RX_32Byte[7]<<24) + (RX_32Byte[6]<<16) + (RX_32Byte[5]<<8) + RX_32Byte[4]); //Bytes 4-7
    	AccumulatedCharge_Time = ((RX_32Byte[11]<<24) + (RX_32Byte[10]<<16) + (RX_32Byte[9]<<8) + RX_32Byte[8]); //Bytes 8-11
    }
    
    // ********************************* End of BQ769x2 Measurement Commands   *****************************************
    
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    /* USER CODE END 0 */
    
    /**
      * @brief  The application entry point.
      * @retval int
      */
    int main(void)
    {
      /* USER CODE BEGIN 1 */
    
      /* USER CODE END 1 */
    
      /* MCU Configuration--------------------------------------------------------*/
    
      /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
      	HAL_Init();
    
      /* USER CODE BEGIN Init */
    
      /* USER CODE END Init */
    
      /* Configure the system clock */
      	SystemClock_Config();
    
      /* USER CODE BEGIN SysInit */
    
      /* USER CODE END SysInit */
    
      /* Initialize all configured peripherals */
      	MX_GPIO_Init();
      	MX_I2C1_Init();
      	MX_USART2_UART_Init();
      	MX_TIM1_Init();
      /* USER CODE BEGIN 2 */
    	// Start timer
    	HAL_TIM_Base_Start(&htim1);
    
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // RST_SHUT pin set low
    	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
      	delayUS(10000);
    HAL_TIM_Base_Start(&htim1);
    	CommandSubcommands(BQ769x2_RESET);  // Resets the BQ769x2 registers
    	delayUS(60000);
    	BQ769x2_Init();  // Configure all of the BQ769x2 register settings
    	delayUS(10000);
    	CommandSubcommands(FET_ENABLE); // Enable the CHG and DSG FETs
    	delayUS(10000);
    	CommandSubcommands(SLEEP_DISABLE); // Sleep mode is enabled by default. For this example, Sleep is disabled to 
    									   // demonstrate full-speed measurements in Normal mode. 
    
    	delayUS(60000); delayUS(60000); delayUS(60000); delayUS(60000);  //wait to start measurements after FETs close
    
      /* USER CODE END 2 */
    
      /* Infinite loop */
      /* USER CODE BEGIN WHILE */
      while (1)
      {
        /* USER CODE END WHILE */
    
        /* USER CODE BEGIN 3 */
    	
        //Reads Cell, Stack, Pack, LD Voltages, Pack Current and TS1/TS3 Temperatures in a loop
    	//This basic example polls the Alarm Status register to see if protections have triggered or new measurements are ready
    	//The ALERT pin can also be used as an interrupt to the microcontroller for fastest response time instead of polling
    	//In this example the LED on the microcontroller board will be turned on to indicate a protection has triggered and will 
    	//be turned off if the protection condition has cleared.
    
    		AlarmBits = BQ769x2_ReadAlarmStatus();
    		if (AlarmBits & 0x80) {  // Check if FULLSCAN is complete. If set, new measurements are available
          		BQ769x2_ReadAllVoltages();
          		Pack_Current = BQ769x2_ReadCurrent();
          		Temperature[0] = BQ769x2_ReadTemperature(TS1Temperature);
          		Temperature[1] = BQ769x2_ReadTemperature(TS3Temperature);
    			DirectCommands(AlarmStatus, 0x0080, W);  // Clear the FULLSCAN bit
    		}
    				
    		if (AlarmBits & 0xC000) {  // If Safety Status bits are showing in AlarmStatus register
    			BQ769x2_ReadSafetyStatus(); // Read the Safety Status registers to find which protections have triggered
    			if (ProtectionsTriggered & 1) {
    				HAL_GPIO_WritePin(GPIOA, LD2_Pin, GPIO_PIN_SET); }// Turn on the LED to indicate Protection has triggered
    				DirectCommands(AlarmStatus, 0xF800, W); // Clear the Safety Status Alarm bits.
    			}
    		else
    		{
    			if (ProtectionsTriggered & 1) {
    				BQ769x2_ReadSafetyStatus();
    				if (!(ProtectionsTriggered & 1)) 
    				{
    					HAL_GPIO_WritePin(GPIOA, LD2_Pin, GPIO_PIN_RESET);
    				} 
    			} // Turn off the LED if Safety Status has cleared which means the protection condition is no longer present
    		}
    		delayUS(20000);  // repeat loop every 20 ms
      }
      /* USER CODE END 3 */
    }
    
    /**
      * @brief System Clock Configuration
      * @retval None
      */
    void SystemClock_Config(void)
    {
      RCC_OscInitTypeDef RCC_OscInitStruct = {0};
      RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
      /** Initializes the RCC Oscillators according to the specified parameters
      * in the RCC_OscInitTypeDef structure.
      */
      RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
      RCC_OscInitStruct.HSEState = RCC_HSE_ON;
      RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
      RCC_OscInitStruct.HSIState = RCC_HSI_ON;
      RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
      RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
      RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8;
      if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
      {
        Error_Handler();
      }
      /** Initializes the CPU, AHB and APB buses clocks
      */
      RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                                  |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
      RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
      RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
      RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
      RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
      if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
      {
        Error_Handler();
      }
    }
    
    /**
      * @brief I2C1 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_I2C1_Init(void)
    {
    
      /* USER CODE BEGIN I2C1_Init 0 */
    
      /* USER CODE END I2C1_Init 0 */
    
      /* USER CODE BEGIN I2C1_Init 1 */
    
      /* USER CODE END I2C1_Init 1 */
      hi2c1.Instance = I2C1;
      hi2c1.Init.ClockSpeed = 400000;
      hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
      hi2c1.Init.OwnAddress1 = 0;
      hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
      hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
      hi2c1.Init.OwnAddress2 = 0;
      hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
      hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
      if (HAL_I2C_Init(&hi2c1) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN I2C1_Init 2 */
    
      /* USER CODE END I2C1_Init 2 */
    
    }
    
    /**
      * @brief TIM1 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_TIM1_Init(void)
    {
    
      /* USER CODE BEGIN TIM1_Init 0 */
    
      /* USER CODE END TIM1_Init 0 */
    
      TIM_ClockConfigTypeDef sClockSourceConfig = {0};
      TIM_MasterConfigTypeDef sMasterConfig = {0};
    
      /* USER CODE BEGIN TIM1_Init 1 */
    
      /* USER CODE END TIM1_Init 1 */
      htim1.Instance = TIM1;
      htim1.Init.Prescaler = 63;
      htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
      htim1.Init.Period = 65535;
      htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
      htim1.Init.RepetitionCounter = 0;
      htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
      if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
      {
        Error_Handler();
      }
      sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
      if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
      {
        Error_Handler();
      }
      sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
      sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
      if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN TIM1_Init 2 */
    
      /* USER CODE END TIM1_Init 2 */
    
    }
    
    /**
      * @brief USART2 Initialization Function
      * @param None
      * @retval None
      */
    static void MX_USART2_UART_Init(void)
    {
    
      /* USER CODE BEGIN USART2_Init 0 */
    
      /* USER CODE END USART2_Init 0 */
    
      /* USER CODE BEGIN USART2_Init 1 */
    
      /* USER CODE END USART2_Init 1 */
      huart2.Instance = USART2;
      huart2.Init.BaudRate = 115200;
      huart2.Init.WordLength = UART_WORDLENGTH_8B;
      huart2.Init.StopBits = UART_STOPBITS_1;
      huart2.Init.Parity = UART_PARITY_NONE;
      huart2.Init.Mode = UART_MODE_TX_RX;
      huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
      huart2.Init.OverSampling = UART_OVERSAMPLING_16;
      if (HAL_UART_Init(&huart2) != HAL_OK)
      {
        Error_Handler();
      }
      /* USER CODE BEGIN USART2_Init 2 */
    
      /* USER CODE END USART2_Init 2 */
    
    }
    
    /**
      * @brief GPIO Initialization Function
      * @param None
      * @retval None
      */
    static void MX_GPIO_Init(void)
    {
      GPIO_InitTypeDef GPIO_InitStruct = {0};
    
      /* GPIO Ports Clock Enable */
      __HAL_RCC_GPIOC_CLK_ENABLE();
      __HAL_RCC_GPIOD_CLK_ENABLE();
      __HAL_RCC_GPIOA_CLK_ENABLE();
      __HAL_RCC_GPIOB_CLK_ENABLE();
    
      /*Configure GPIO pin Output Level */
      HAL_GPIO_WritePin(GPIOA, LD2_Pin|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10, GPIO_PIN_RESET);
    
      /*Configure GPIO pin : B1_Pin */
      GPIO_InitStruct.Pin = B1_Pin;
      GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
      GPIO_InitStruct.Pull = GPIO_NOPULL;
      HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
    
      /*Configure GPIO pins : LD2_Pin PA8 PA9 PA10 */
      GPIO_InitStruct.Pin = LD2_Pin|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10;
      GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
      GPIO_InitStruct.Pull = GPIO_NOPULL;
      GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
      HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
      /* EXTI interrupt init*/
      HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
      HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
    
    }
    
    /* USER CODE BEGIN 4 */
    
    /* USER CODE END 4 */
    
    /**
      * @brief  This function is executed in case of error occurrence.
      * @retval None
      */
    void Error_Handler(void)
    {
      /* USER CODE BEGIN Error_Handler_Debug */
      /* User can add his own implementation to report the HAL error return state */
    
      /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef  USE_FULL_ASSERT
    /**
      * @brief  Reports the name of the source file and the source line number
      *         where the assert_param error has occurred.
      * @param  file: pointer to the source file name
      * @param  line: assert_param error line source number
      * @retval None
      */
    void assert_failed(uint8_t *file, uint32_t line)
    {
      /* USER CODE BEGIN 6 */
      /* User can add his own implementation to report the file name and line number,
         tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
      /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */
    
    /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
    
    
    
    
    
    
    
    
    
    
    
    
     

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Arjun:

    TI 的所有示例代码均可在以下位置找到: https://www.ti.com/lit/zip/sluc701。 除此之外、我还有几个简短的问题。

    over uart

    1.您想使用 UART 连接什么设备? BQ769x2系列不包含 UART 接口。

    BQ79XXX

    2.您是否正在尝试使用 BQ769x2或 BQ79xxx 器件? 每个都需要不同的代码/寄存器。

    3. BQ769x2的原理图中是否包含 I2C 的上拉电阻器?

    4.您是否有我可以为您的设置查看的原理图?

    此致!

    A·内德尔费尔德