This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM5001:TI 直流/直流反激式控制芯片的选择建议

Guru**** 2668435 points

Other Parts Discussed in Thread: LM5155, LM5158, LM5156

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1340857/lm5001-selection-suggestions-for-ti-dc-dc-flyback-control-chip

器件型号:LM5001
主题中讨论的其他器件:LM5158LM5156、LM5155

您好!

我想将 TI 反激式控制器(输出功率15W、无需外部 MOSFET)用于具有3个输出的直流/直流反激式转换器300mA、其中两个不是隔离的(3.3V/2A 和12V/MOSFET)、其中一个是隔离的(100mA)。 我希望在不使用光耦合器的情况下直接通过非隔离式输出(3.3V/2A)进行调节。 总输出功率为11.4W。 输入电压范围为16VDC-60VDC。

非常感谢。