This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PFCLLCSREVM034:最大功率问题

Guru**** 2785785 points

Other Parts Discussed in Thread: UCC28056, UCC256404

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1348229/pfcllcsrevm034-maximum-power-issue

器件型号:PFCLLCSREVM034
主题中讨论的其他器件:UCC28056UCC256404

您好!

根据"PFCLCSREVM034用户指南"文档、最大设计功率为12V/14A/168W。

我目前遇到的情况是:

当输入为110VAC负载为10.5A 时、它可以平稳启动、当负载超过10.5A 时启动、并会在大约3到10秒后关闭和重新启动。

当输入为220VAC负载为15A 时、它可以平稳启动、而不存在上述问题。

所以我想把最大功率增加到180W、甚至200W?

1.需要更换哪些部件?

2.或者有没有办法解决低电压功率不足的问题?

此致