请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TL494 大家好、
请确认原理图、TL494用于 CC/CV 充电器控制器(适用于超级电容器或电池)、VIN 9V ~ 36V/Vo 5.1V (超级电容器) Vo 4.2V (电池)/IO 1A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.