请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS745-Q1 高级专家
我有一个关于反馈电阻器(R1,R2)需要你的固件的问题。
您是否对 R1 20K、R2 4.02K 的更改有意见?
R1 49.9K,R2 10K
Venthrough 满足 R1+R2< VOUT /(IFB*100)的要求
输入电压为5V、VOUT 为3.3V

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
高级专家
我有一个关于反馈电阻器(R1,R2)需要你的固件的问题。
您是否对 R1 20K、R2 4.02K 的更改有意见?
R1 49.9K,R2 10K
Venthrough 满足 R1+R2< VOUT /(IFB*100)的要求
输入电压为5V、VOUT 为3.3V