This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 如果只需要简单的 CC/CV 功能~可以使用哪种降压解决方案?

Guru**** 2779905 points

Other Parts Discussed in Thread: LM25116

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1222060/if-just-want-a-simple-cc-cv-function-which-step-down-solution-can-be-used

主题中讨论的其他器件:LM25116

大家好、

如果只需要简单的 CC/CV 功能~可以使用哪种降压解决方案?

输入电压=20V  

电压= 15.6V

IO 有2项规格。

Io=1.25A

Io=5A  

2型