This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS563200:TPS563200是否可以从输入12V 输出+5V@3A 和-5V@500mA?

Guru**** 2540720 points
Other Parts Discussed in Thread: TPS563200

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1212303/tps563200-is-it-possible-for-tps563200-to-output-5v-3a-and--5v-500ma-from-input-12v

器件型号:TPS563200

TPS563200是否可以从输入12V 输出+5V@3A 和-5V@500mA?

以下原理图是否正常?