请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS55010 大家好、我希望开发一款输入为3.3V、输出为12V、最大输出电流为50 mA 的隔离式 DC-DC。 其主要考虑因素是在输出端无任何负载时从输入端汲取的低待机电流-低于500uA。
这可以通过 TPS55010实现吗?或者我是否需要使用任何其他芯片组?
此致、Prithvi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.