请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25756 工具与软件:
您好!
我正在查看 BQ25756的数据表、其中表明、锂离子电池最多可以支持14节电池(磷酸铁锂电池为16节)。 同时、它的额定工作电池电压高达70V。 但考虑到最大锂离子电池电压为每节4.2V、16节电池组只能达到67.2V。 这是否意味着 BQ25656也可用于16节锂离子电池组?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.