请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS53679 工具与软件:
您好、TI 大师
我有一个问题:
TPS53679定义了上电顺序、即在12V 之前上电5V。
但参考设计:12V 在5V 之前。
问题:如果在12V 之后5V 可以上电?
谢谢!



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.