This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPSM863252:器件推荐

Guru**** 2927270 points

Other Parts Discussed in Thread: UCD9090-Q1, TPSM863252

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1389247/tpsm863252-part-recommendations

器件型号:TPSM863252
主题中讨论的其他器件:UCD9090-Q1

工具与软件:

我有一些直流/直流电源稳压器需求、我希望 TI 可以推荐最佳的直流/直流非隔离匹配方案。  输入将是+5V。

 

  1. 0.88V、25A、3%(1%直流精度+ 2%交流纹波)、阶跃响应9A 超过350ns、斜升时间≤5ms。
  2. 0.8V、4A、3%直流精度、斜升时间≤3ms
  3. 1.2V、500mA、3%直流精度、斜升时间≤5ms (可能是由1.8V 馈电的 LDO)
  4. 1.8V、2A、3%直流精度、斜升时间≤3ms
  5. 3.3V、2A、3%直流精度、斜升时间≤5ms

稳压器将由 UCD9090-Q1进行管理/时序控制