请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2069E 工具与软件:
你(们)好
客户在 USB3上使用 FP6861。 1.5A 是保护电流、但 FP6861的裕度为1.7A。
我想问一下标记为1.5A 的 TPS2069E 是否与 FP6861具有相同的裕度以达到1.7A。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.