This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ25731:BQ25731是否可以支持超级电容器备用功能?

Guru**** 2387970 points
Other Parts Discussed in Thread: BQ25731, BQ24800
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1404723/bq25731-can-bq25731-support-supercapacitor-backup-function

器件型号:BQ25731
Thread 中讨论的其他器件: BQ24800

工具与软件:

大家好、团队成员:

我需要  超级电容器备用功能(电源输入为12V、器件电源也为12V、超级电容器为5.5V)、我想知道  BQ25731是否可以支持以下功能:

1.输入12V 电源供电时,VSYS 为设备供电(电压也是12V)并为5.5V 超级电容器降压

2.在没有输入源的情况下、超级电容通过升压 电路为 VSYS 供电(升压电压范围为7V-12V)

请帮助检查 BQ25731是否可以支持此功能、如果可以、如何配置寄存器?