Other Parts Discussed in Thread: LMR38025
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR38025 工具与软件:
你(们)好。
如果可以使用 LMR38025将12V 转换为-38V 负电压? 负载电流小于200mA。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.