Other Parts Discussed in Thread: TPS51200
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS51200 工具与软件:
你(们)好
请帮助查看 下面的设计并提供您的反馈。
器件型号:TPS51200
输入电压:2.5V
REF 输入:1.2V
输出电压:0.6V
负载电流:650mA

提前感谢、
此致
Haritha.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.