请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ40Z80 Thread 中讨论的其他器件:BQSTUDIO
工具与软件:
您好!
在放电期间、当电芯电压降至2.5V (CUV 阈值设置为2500mV)时、XDSG 标志变为1 (正常)、但放电永不停止。
请、需要更改哪个参数以切断放电?
此致。
Philippe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.