请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLC59208F Thread 中讨论的其他器件:TPS61199
工具与软件:
亮度水平比
例如、在 TPS61199上(200Hz 时的 PWM 调光比为5000:1)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.