This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS65131:TPS

Guru**** 2782575 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1441257/tps65131-tps

器件型号:TPS65131

工具与软件:

您好!

我希望将18V 至25.2V 的电池电压转换为+/- 25V 至+/- 48V 的双极性电压(可调)、输出电流至少为5A。

输入电压:18至30V 直流

输出1:25至48V  

输出2:-25V 至- 48V

可调节输出电流:5A 至10A

尺寸:70m x 50mm x 25mm

请告诉我哪些部件非常适合。