This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS650861:PMIC 要求

Guru**** 2813935 points

Other Parts Discussed in Thread: LP8758-EA

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1453722/tps650861-pmic-requirement

器件型号:TPS650861
Thread 中讨论的其他器件:LP8758-EA

工具与软件:

您好!

目前、我在设计中使用了两个 IRPS5401、它有四相、因此 A 相和 B 相支持高达2A、C 相和 D 相支持高达4A。

我需要的是输入= 3.3V 且输出= 1.1V (DUT 电源)、0.9V (DUT 电源)、1.8V (DUT 数字电源)、1.8V (DUT 模拟电源)、1.8V (平台电源)、2.5V (DUT 电源轨)、2.5V (DUT 电源轨)、每个电源轨的电流= 4A。

您是否可以为上述要求建议一个确切的替代件?