This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ25629:额外/意外的 ADC 完成中断

Guru**** 2811985 points

Other Parts Discussed in Thread: BQ25629, BQ25620, BQ25629EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1467979/bq25629-extra-unexpected-adc-done-interrupts

器件型号:BQ25629
主题中讨论的其他器件: BQ25620

工具与软件:

在我们的 Linux 电池驱动程序(从 TI 获取但我们为 BQ25629进行了修改的 BQ25620/2驱动程序)中、我已将以下代码添加到中断处理程序:

 // clear flags
ret = regmap_read(bq->regmap, BQ2562X_CHRG_FLAG_0, &val);
if (ret) {
dev_err(bq->dev, "Error reading chrg_flag_0: %d", ret);
} else if (val) {
dev_dbg(bq->dev, "Charger flag 0 0x%x", val);
}
ret = regmap_read(bq->regmap, BQ2562X_CHRG_FLAG_1, &val);
if (ret) {
dev_err(bq->dev, "Error reading chrg_flag_1: %d", ret);
} else if (val) {
dev_dbg(bq->dev, "Charger flag 1 0x%x", val);
}
ret = regmap_read(bq->regmap, BQ2562X_FAULT_FLAG_0, &val);
if (ret) {
dev_err(bq->dev, "Error reading fault_flag_0: %d", ret);
} else if (val) {
dev_dbg(bq->dev, "Fault flag 0x%x", val);
}

我想了解为什么会不断触发中断处理程序。  结果是 CHARGER_FLAG_0返回0x40、即 ADC_DONE_FLAG。  
我不知道为什么这个中断会持续触发。  因此、我进一步将 Charger_Mask_ 0设置为0x40、以按推测屏蔽此中断。
但是、我们仍会不断获得中断、并始终设置 ADC_DONE。
我们使用的是单次触发 ADC 模式、在触发这些中断时不会设置 ADC_en 位。  禁用这些中断的正确方法是什么?
以下是来自 i2c 的原始寄存器转储:
00: ff
01: ff
02: 40
03: 06
04: a0
05: 0d
06: 00
07: 0a
08: e0
09: 0e
0a: 20
0b: 03
0c: c0
0d: 0f
0e: 00
0f: 0b
10: 80
11: 00
12: 20
13: 00
14: 04
15: 1c
16: a0
17: 4f
18: 04
19: c0
1a: 3d
1b: 25
1c: 3f
1d: 40
1e: 00
1f: 04
20: 04
21: 00
22: 00
23: 40
24: 00
25: 00
26: 70
27: 00
28: 68
29: 01
2a: 00
2b: 00
2c: f8
2d: 12
2e: e4
2f: 12
30: 9e
31: 10
32: 9a
33: 10
34: cd
35: 01
36: 49
37: 00
38: 32
下面是从该转储解析的输出(如果我已正确解释寄存器):
0x2: Charge Current Limit: 2000mA
0x4: Charge Voltage Limit: 4360mV
0x6: Input Current Limit: 3200mA
0x8: Input Voltage Limit: 4760mV
0xc: VOTG Regulation: 5040mV
0xe: Minimal System Voltage: 0xb00: 3520mV
0x10: Precharge Current Regulation: 160mA - TODO if q4_fullon=1 min is 80mA
0x12: Termination Current Threshold: 40mA - TODO if q4_fullon=1 min is 60mA
0x14: Charge Control: (0x4)
 Q1_FULLON: 0
 Q4_FULLON: 0
 ITRICKLE: 10mA
 top-off timer: disabled
 Enable Termination: 1
 VINDPM_BAT_TRACK: VBAT+400mV
 Recharge Threshold offset: 200mV
0x15: Charge Timer Control: (0x1c)
 disable stat pin: 0
 Auto D+/D- detect: 0
 Force D+/D- detect: 0
 Enable DCP Bias: 1
 2x timer en: 1
 en safety timers: 1
 precharge safety timer: 0.62 hrs
 fast charge safety timer: 28 hrs
0x16: Charge Control 0: (0xa0)
 Auto OVP discharge: 1
 Force Discharge: 0
 Charge Enable: 1
 En HiZ: 0
 Force PMID discharge : 0
 wd timer reset: 0
 watchdog timer: disable
0x17: Charge Control 1: (0x4f)
 Reset: 0
 Therm Reg threshold: 120C
 Converter switching freq: 1.5Mhz (default)
 Converter drive stength: strong (default)
 VBus OVP: 18.5V
0x18: Charge Control 2: (0x4)
 Boost Bypass: 0
 OTG enable: 0
 Disable PFM in Boost Mode: 0
 Disable PFM in Forward buck mode: 0
 BATFET ctrl wvbus: 0
 BATFET ctrl delay time: 10s
 BATFET ctrl: normal
0x19: Charge Control 3: (0xc0)
 Peak discharge current protection: 12A
 VBat UVLO, Short: UVLO=2.2V Short=2.05V
 VBat OTG Min: 3V rising 2.8V falling
 Charge Rate: 1C
0x1a: NTC Control 0: (0x3d)
 TS Ignore: 0
 TS Hot Thresh: 60C
 TS Cold Thresh: -10C
 TS Warm ICHG: Unchanged
 TS Cool ICHG: 20%
0x1b: NTC Control 1: (0x25)
 Falling TH1,2,3 Thres: (0, 10, 15)C
 Rising TH4,5,6: (35, 45, 60)C
 TS warm voltage: VREG-200mV
0x1c: NTC Control 2: (0x3f)
 TS_VSET_SYM: 0
 TS_VSET_PREWARM: unchanged
 Prewarm Current (TH4,5): unchanged
 Precool Current (TH2,3): unchanged
0x1d: Charger Status 0: 0x40)
 ADC Conversion Status: 1
 Device in thermal regulation: 0
 VSys regulation: BAT > VSYSMIN
 IINDPM_STAT: Normal
 VINDPM_STAT: Normal
 Safety Timer Expired: 0
 Watchdog Timer Expired: 0
0x1e: Charger Status 1: 
 Charge Status: Not charging
 VBus Status: No qualified adapter or EN_AUTO_INDET=0
0x1f: Fault Status 0: (0x4)
 VBUS Fault: Normal
 Batt Fault: Normal
 VSys Stat: Normal
 OTG Fault Stat: 0
 Thermal Shutdown: 0
 TS Zone: Warm
0x20: Charger Flag 0: 0x4
 ADC Done: 0
 Thermal Regulation: 0
 VSYS Min Regulation: 0
 IINDPM: 0
 VINDPM: 1
 Safety Timer: 0
 Watchdog: 0
0x21: Charger Flag 1: 0x0
 Charge Status Changed: 0
 VBus Changed: 0
0x22: Fault Flag 0: 0x0
 VBus OVP or Sleep: 0
 VBat OCP or OVP: 0
 VSYS Over voltage or SYS short: 0
 OTG Over voltage or fault: 0
 TS Shutdown: 0
 TS Status Change: 0
0x23: Charger Mask 0: 0x40
0x24: Charger Mask 1: 0x0
0x25: Fault Mask 0: 0x0
0x26: ADC Control: (0x70)
 ADC En: 0
 ADC Rate: One Shot
 ADC Speed: 9 bit
 ADC Avg ctl: Single
 ADC Avg initial: Existing value
0x27: ADC Disables: 0x0
0x28: IBUS ADC: 360mA
0x2a: IBAT ADC: 0mA
0x2c: VBUS ADC: 4819.58mV
0x2e: VMMID ADC: 4799.7300000000005mV
0x30: VBAT ADC: 4232.73mV
0x32: VSYS ADC: 4228.75mV
0x34: TS ADC: 44.3021%
0x36: TDIE ADC: 36.5C
0x38: Part Info: 
 Part Number BQ25629
 Revision: 2
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Dennis:  

    请查看我的以下评论。  

    我已经尝试复制您在 BQ25629EVM 上的观察结果、但我观察到与 ADC_DONE_FLAG 和设置 ADC_DONE_MASK 相关的预期行为。  仅在 ADC_EN 初始化 ADC 转换后才设置 ADC_DONE_FLAG、当我将 Charger_Mask_ 0设置为0x40时、在单次触发模式下重复开启 ADC 时、不再看到任何中断。  

    鉴于此、我有几个后续问题。  

    -能否确认  如果将 ADC 模式更改为连续模式、是否不再设置 ADC_DONE_FLAG?

    -参考寄存器转储状态寄存器指示 TS_WARM、充电状态指示未充电/充电终止。 我想知道您看到的任何中断是否可能是器件停止充电或在 TS_NORMAL 与 TS_WARM 之间变化所致。  

    另一种可能是您在无意中启用了代码中的 ADC。 目前、我们尚未收到任何其他中断报告或 ADC_DONE_FLAG 在此器件上无法正常工作。  

    此致、

    Garrett

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    很抱歉、我尝试删除此帖子。  我在调试过程中犯了一个错误、导致这个问题出现了错误。  这不是我所报告的、我们的 ADC_DONE 正常工作。  感谢您的观看。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Dennis:  

    不用担心、感谢您确认您实际上没有看到  ADC_DONE_FLAG 存在问题。  

    此致、

    Garrett