This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] UCC5880-Q1:爬电分立与 IEC 60664-1

Guru**** 2542940 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1469208/ucc5880-q1-creepage-disctance-vs-iec-60664-1

器件型号:UCC5880-Q1

工具与软件:

您好!

该器件的外部爬电距离为8mm。 根据 IEC 60664-1850V 系统要求4.3mm。
因此、安全隔离(双基极隔离)意味着8.6mm 的距离、这超出了数据表中的规定。

TI 如何辩称此器件可用于850V 甚至1000V 应用?

此致