This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] UCD3138128:多图像编程

Guru**** 2771175 points

Other Parts Discussed in Thread: UCD3138128A, UCD3138128, UCD3138064

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1473463/ucd3138128-multiple-image-progamming

器件型号:UCD3138128
主题中讨论的其他器件:UCD3138064

工具与软件:

我将编写一些代码、以允许通过串行端口对 UCD3138128A 进行编程。

我的问题是

要使启动代码识别块2和3中的映像、需要做些什么才能在启动时也进行切换。

然后... 当我使用较新的映像对这些块进行编程时、如何使其再次切换到块0和1?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好、蝙蝠侠:

    我正在审核您的问题、我将在星期五回复。

    此致、

    Jonathan Wong

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好、蝙蝠侠:

    UCD3138FW-BIDI 有一个清除 UCD3138128上的块0 - 3的示例。  

    main.c 在 BIDIRECTION_DC-UCD3138128中具有  clear_integrity_words()  (第110行)基于参数清除块0 - 3的函数。  

    #if (UCD3138128 )
    	#ifdef MEMORY_SCRUBBING
    					clear_integrity_word(1);		// erase 8-byte checksum @ end of pflash block 1
    				  //clear_integrity_word(3);		// erase 8-byte checksum @ end of pflash block 3
    					reset_uP();
    	#else
    					clear_integrity_word(0);
    	#endif

    software_interrupt_wrapper.c 显示 clear_integrity_words()触发软件中断情况12 (第95行)。  

    void clear_integrity_word(Uint32 block)
    {
         swi_single_entry(block,0,0,12);
    }

    interrupts.c 包含软件中断处理程序。 In 案例12. (第163行)、代码通过清除相应的用户校验和来清除编程闪存块。

    case 12: // clear integrity words, depending on arg1
    
    #if (UCD3138128)
    		//Note:  This clear integrity word covers all cases.  It is designed to clear integrity words based on what address the flash block is
    				//mapped to when it is called.  This is done for code which switches blocks.  And it can erase the integrity word at the end of each of 4 blocks.
    				//
    				//For most applications, it can be simplified considerably if code space is scarce
    				//
    				//
    	{
    		register Uint32 * program_index = (Uint32 *) program_area; //store destination address for program
    					register Uint32 * source_index = (Uint32 *) zero_out_integrity_double_word; //Used for source address of PFLASH;
    
    					register Uint32 counter;
    
    					if(arg1 == 0) //0 means first block in memory, regardless of which block that is;
    					{
    						zoiw_address = 0x7ff8;
    
    						if((DecRegs.MFBALR1.bit.ADDRESS == 0) && (DecRegs.MFBAHR1.bit.ADDRESS == 0)) //here if flash block 0 is at 0
    						{
    							zoiw_flash_key = PROGRAM_FLASH0_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR17.bit.ADDRESS == 0) && (DecRegs.MFBAHR17.bit.ADDRESS == 0))//if it's program flash 1;
    						{
    							zoiw_flash_key = PROGRAM_FLASH1_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR18.bit.ADDRESS == 0) && (DecRegs.MFBAHR18.bit.ADDRESS == 0))//if it's program flash 2;
    						{
    							zoiw_flash_key = PROGRAM_FLASH2_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR19.bit.ADDRESS == 0) && (DecRegs.MFBAHR19.bit.ADDRESS == 0))//if it's program flash 3;
    						{
    							zoiw_flash_key = PROGRAM_FLASH3_INTERLOCK_KEY;
    						}
    						else
    						{
    							return;
    						}
    					}
    					else if(arg1 == 1)//1 means end of second block;
    					{
    						zoiw_address = 0xfff8;
    
    						if((DecRegs.MFBALR1.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR1.bit.ADDRESS == 0)) //here if flash block 0 is at 0x8000
    						//note that the address bits start at bit 10, so 0x20 in the address field equals 0x8000
    						{
    							zoiw_flash_key = PROGRAM_FLASH0_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR17.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR17.bit.ADDRESS == 0))//if it's program flash 1;
    						{
    							zoiw_flash_key = PROGRAM_FLASH1_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR18.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR18.bit.ADDRESS == 0))//if it's program flash 2;
    						{
    							zoiw_flash_key = PROGRAM_FLASH2_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR19.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR19.bit.ADDRESS == 0))//if it's program flash 3;
    						{
    							zoiw_flash_key = PROGRAM_FLASH3_INTERLOCK_KEY;
    						}
    						else
    						{
    							return;
    						}
    					}
    					else if(arg1 == 2) //2 means end of third block in memory, regardless of which block that is;
    					{
    						zoiw_address = 0x17ff8;
    
    						if((DecRegs.MFBALR1.bit.ADDRESS == 0) && (DecRegs.MFBAHR1.bit.ADDRESS == 1)) //here if flash block 0 is at 0x10000
    						{
    							zoiw_flash_key = PROGRAM_FLASH0_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR17.bit.ADDRESS == 0) && (DecRegs.MFBAHR17.bit.ADDRESS == 1))//if it's program flash 1;
    						{
    							zoiw_flash_key = PROGRAM_FLASH1_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR18.bit.ADDRESS == 0) && (DecRegs.MFBAHR18.bit.ADDRESS == 1))//if it's program flash 2;
    						{
    							zoiw_flash_key = PROGRAM_FLASH2_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR19.bit.ADDRESS == 0) && (DecRegs.MFBAHR19.bit.ADDRESS == 1))//if it's program flash 3;
    						{
    							zoiw_flash_key = PROGRAM_FLASH3_INTERLOCK_KEY;
    						}
    						else
    						{
    							return;
    						}
    					}
    					else if(arg1 == 3)//2 means end of fourth block;
    					{
    						zoiw_address = 0x1fff8;
    
    						if((DecRegs.MFBALR1.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR1.bit.ADDRESS == 1)) //here if flash block 0 is at 0x18000
    						//note that the address bits start at bit 10, so 0x20 in the address field equals 0x8000
    						{
    							zoiw_flash_key = PROGRAM_FLASH0_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR17.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR17.bit.ADDRESS == 1))//if it's program flash 1;
    						{
    							zoiw_flash_key = PROGRAM_FLASH1_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR18.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR18.bit.ADDRESS == 1))//if it's program flash 2;
    						{
    							zoiw_flash_key = PROGRAM_FLASH2_INTERLOCK_KEY;
    						}
    						else if((DecRegs.MFBALR19.bit.ADDRESS == 0x20) && (DecRegs.MFBAHR19.bit.ADDRESS == 1))//if it's program flash 3;
    						{
    							zoiw_flash_key = PROGRAM_FLASH3_INTERLOCK_KEY;
    						}
    						else
    						{
    							return;
    						}
    					}
    					else
    					{
    						return; //reject other arg1 values
    					}
    
    					for(counter=0; counter < 32; counter++) //Copy program from PFLASH to RAM
    					{
    						*(program_index++)=*(source_index++);
    					}
    
    					DecRegs.MFBALR1.bit.RONLY = 0; //enable program flash 1 write
    					DecRegs.MFBALR17.bit.RONLY = 0; //enable program flash 2 write
    
    					{
    						register FUNC_PTR func_ptr;
    						func_ptr=(FUNC_PTR)program_area;     //Set function to program area
    						func_ptr();
    
    					}        //execute erase checksum
    
    					DecRegs.MFBALR1.bit.RONLY = 1; //restore it to read only
    					DecRegs.MFBALR17.bit.RONLY = 1; //restore it to read only
    		            SysRegs.SYSECR.bit.RESET = 2;   //now reset processor.
    					break;
    
    	}

    用户校验和地址 基于 UCD31xx TRM 第469页的。 请参阅表以直观查看程序闪存和用户校验和地址的概述。  

    您可以使用这些地址清除和切换不同的程序闪存块。

    我认为、您用于在程序闪存块之间进行切换的应用仅用于动态更新。 如果是、我们确实提供了我可以共享的动态更新固件示例、尽管该固件适用于 UCD3138064而不是 UCD3138128A。 如果您有兴趣、请告诉我、我可以直接向您发送文件。

    以下是介绍一般动态/无线(OTA)更新的文章: https://www.electronicproducts.com/on-the-fly-power-supply-firmware-upgrades/?terms=Ian+Bower 

    e2e.ti.com/.../On_2D00_the_2D00_fly-power-supply-firmware-upgrades.docx

    下面是一些其他可能有用的 E2E 主题:

    此致、

    Jonathan Wong