This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 关于:PROCESSOR-SDK-AM64X:在适用于 AM64X 的 Processor SDK Linux 中删除和添加封装

Guru**** 2457340 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1493716/re-processor-sdk-am64x-removing-and-adding-packages-in-processor-sdk-linux-for-am64x

谢谢您 

您好、Andreas、

我在 AM64xx EVM 上遇到 xHCI 主机控制器超时问题。 错误消息如下所示:

[   11.272609] usbcore: registered new interface driver usbfs
[   11.304515] usbcore: registered new interface driver hub
[   11.354920] usbcore: registered new device driver usb
[   11.551351] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[   11.557242] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1                                                                                         am64xx-evm login: [   21.572530] xhci-hcd xhci-hcd.0.auto: can't setup: -110
[   21.577883] xhci-hcd xhci-hcd.0.auto: USB bus 1 deregistered
[   21.586559] xhci-hcd: probe of xhci-hcd.0.auto failed with error -110

我已尝试重新启动系统并检查连接、但问题仍然存在。 您能否提供有关如何解决此错误的指导?

谢谢你