主题中讨论的其他器件:AM625
工具与软件:
您好、TI
我最近一直在调试 U-boot 启动界面功能、我想回答两个问题。
1.背景:我们的定制开发板有两个型号,使用 RGB888接口和单个 LVDS 接口视频。 两个定制电路板都使用 EMMC UDA 原始模式引导。
2.遇到的问题:
(1)当我在 uboot 命令行上执行'bmp display $loadaddr m m'命令时、会报告以下错误。 我在 e2e 上看到了一些帖子、似乎 TI 仅在双 LVDS 接口上进行了验证?
=> ls mmc 0 /boot
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 4096 dtb
20212224 Image
12285 ti_logo_414x97_32bpp.bmp.gz
=> ext4load mmc 0 $loadaddr /boot/ti_logo_414x97_32bpp.bmp.gz
This will not be a case any time
12285 bytes read in 18 ms (666 KiB/s)
=> bmp display $loadaddr m m
single-pinctrl pinctrl@f4000: configuring pins for main-dss0-pins-default
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4100/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40f8/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4104/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40fc/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40b8/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40bc/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40c0/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40c4/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40c8/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40cc/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40d0/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40d4/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40d8/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40dc/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40e0/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40e4/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40e8/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40ec/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40f0/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f40f4/0x00010000
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f405c/0x00010001
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4060/0x00010001
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4064/0x00010001
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4068/0x00010001
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f406c/0x00010001
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4070/0x00010001
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4074/0x00010001
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f4078/0x00010001
ti_ehrpwm pwm@23010000: regs=0x23010000
single-pinctrl pinctrl@f4000: configuring pins for main-epwm1-a-pins-default
single-pinctrl pinctrl@f4000: reg/val 0x00000000000f419c/0x00010006
tidss_drv dss@30200000: vidl1: bufsize 2560, buf_threshold 2559/1280, mflag threshold 1706/853 preload 1280
tidss_drv dss@30200000: vid1: bufsize 2560, buf_threshold 2559/1280, mflag threshold 1706/853 preload 1280
tidss_drv dss@30200000: vp1: new rate 51923076 Hz (requested 51912000 Hz)
tidss_drv dss@30200000: dss_vp_set_gamma: hw_videoport 1, lut len 0, hw len 256
tidss_drv dss@30200000: dss_vp_write_gamma_table: hw_videoport 1
tidss_drv dss@30200000: DSS fclk 250000000 Hz
"Synchronous Abort" handler, esr 0x96000004
elr: 000000008086a114 lr : 000000008086ce14 (reloc)
elr: 000000009b64e114 lr : 000000009b650e14
x0 : 0000000000000000 x1 : 0001010100000000
x2 : 000000000000000a x3 : 0000000002800000
x4 : 0000000002800000 x5 : 00000000995b4529
x6 : 0000000000000030 x7 : 00000000995b49b0
x8 : 000000000000000c x9 : 0000000000000008
x10: 00000000ffffffe0 x11: 0000000000000006
x12: 000000000001869f x13: 0000000000000000
x14: 0000000000000000 x15: 0000000000000000
x16: 000000009b64bbb0 x17: 00000000996d8f00
x18: 00000000995c4d80 x19: 000000009b6a7b20
x20: 0000000000000000 x21: 00000000995c7f50
x22: 000000009b6c8a71 x23: 000000009b6c75c0
x24: 00000000995baeb8 x25: 0000000000000355
x26: 00000000995cd360 x27: 0000000000000500
x28: 0000000000000002 x29: 00000000995b49c0
Code: d65f03c0 128002a0 17fffffa f9400001 (f9403421)
Resetting CPU ...
resetting ...
(__LW_AT__2)由于我们的启动模式为 EMMC UDA 原始模式、因此我已修改"board/ti/am62x/evm"。 C'。 如下所示、我更改了"的值。 flags 中的所有其他"标识和特性"、将结构数组第二项中的"声明"从"SPLASH_STORAGE-RAW" FS 更改为"SPLASH_STORAGE-RAW"。 我已经编写了命令'ext4load MMC 0 $loadaddr/boot/tilog_414x97_32bpp。 BMP。 GZ"写入 uboot 的环境变量中、但根据 uboot 启动日志、在执行 uboot 命令之前、uboot 已报告错误"错误的 gzipped 数据在给定地址没有有效的 bmp 文件"。 TI 是否验证了 EMMC 的"SPLASH_STORAGE-RAW"? 如果是、如何加载 ti-logo_414x97_32bpp.bbm.gz?
static struct splash_location default_splash_locations[] = {
{
.name = "sf",
.storage = SPLASH_STORAGE_SF,
.flags = SPLASH_STORAGE_RAW,
.offset = 0x700000,
},
{
.name = "mmc",
.storage = SPLASH_STORAGE_MMC,
.flags = SPLASH_STORAGE_RAW,
.devpart = "0:1",
},
};
U-Boot SPL 2023.04-00007-g639d43ac-dirty (Mar 05 2025 - 17:55:17 +0800) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)') SPL initial stack usage: 13408 bytes Trying to boot from MMC1 Authentication passed Authentication passed Authentication passed Loading Environment from nowhere... OK init_env from device 9 not supported! Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2023.04-00007-g639d43ac-dirty (Mar 06 2025 - 17:04:44 +0800) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)') SPL initial stack usage: 1856 bytes Error: Bad gzipped data There is no valid bmp file at the given address Trying to boot from MMC1 Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices U-Boot 2023.04-00007-g639d43ac-dirty (Mar 06 2025 - 17:50:29 +0800) SoC: AM62X SR1.0 HS-FS Model: Texas Instruments AM62x HMI DRAM: 512 MiB Core: 64 devices, 34 uclasses, devicetree: separate MMC: mmc@fa10000: 0 Loading Environment from nowhere... OK Error: Bad gzipped data There is no valid bmp file at the given address In: serial Out: serial Err: serial Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0(part 0) is current device ...................env test1........................... This will not be a case any time 12285 bytes read in 18 ms (666 KiB/s) SD/MMC found on device 0 Failed to load 'boot.scr' Can't set block device echo ...................env test2........................... This will not be a case any time 12285 bytes read in 18 ms (666 KiB/s) ## Error: "main_cpsw0_qsgmii_phyinit" not defined This will not be a case any time 20212224 bytes read in 807 ms (23.9 MiB/s) This will not be a case any time 57631 bytes read in 21 ms (2.6 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000