Thread 中讨论的其他器件: TDA4VH、 TDA4VM
工具/软件:
您好 TI、
我们正在开发基于 TDA4VH 的定制板、并使用 PROCESSOR-SDK-J784S4 v10。
我们正在执行 ECU、CSI_TX1实例的启动、并面临以下问题:
- 我们确实有 vision_apps /从文件读取和转发到 CSITX vision_app 上传: /cfs-file/__key/communityserver-discussions-components-files/791/app_5F00_csitx-_2800_1_2900_.zip (修改后的应用程序从此链接: e2e.ti.com/.../tda4vh-q1-csitx-output-image-abnormally )
- 另一方面、我们使用具有相应解串器的 CSI-RX、并且该器件经过测试、因为摄像头在相同解串器下运行正常。
- 请注意、我们使用的是 MAX 串行器/解串器(4通道、每通道1.5Gbps)
- I2C 总线通过这条线路在 GMSL2链路中正常工作。
当我们在两侧运行应用时(首先运行 Rx 端、然后运行 TX 端)、RX 端不会接收任何内容。
- 捕获状态显示4帧(默认错误缓冲区)。
- 在 CSI_TX 端、我们在 while 循环中发送原始图像。 在应用程序执行期间、日志中未报告故障。
- 下面是 TDA4寄存器与 devmem2的打印输出 :
root@j784s4-evm:~# devmem2 0x04414000 /dev/mem opened. Memory mapped at address 0xffff844e2000. Read at address 0x04414000 (0xffff844e2000): 0x021A202C root@j784s4-evm:~# devmem2 0x04414004 /dev/mem opened. Memory mapped at address 0xffff948b2000. Read at address 0x04414004 (0xffff948b2004): 0x000000A0 root@j784s4-evm:~# devmem2 0x04414008 /dev/mem opened. Memory mapped at address 0xffff8f634000. Read at address 0x04414008 (0xffff8f634008): 0x0000000F root@j784s4-evm:~# devmem2 0x0441400C /dev/mem opened. Memory mapped at address 0xffff7fa69000. Read at address 0x0441400C (0xffff7fa6900c): 0x0000F0F0 root@j784s4-evm:~# devmem2 0x04414010 /dev/mem opened. Memory mapped at address 0xffff9e33f000. Read at address 0x04414010 (0xffff9e33f010): 0x00000000 root@j784s4-evm:~# devmem2 0x04414014 /dev/mem opened. Memory mapped at address 0xffff80ad2000. Read at address 0x04414014 (0xffff80ad2014): 0x00000000 root@j784s4-evm:~# devmem2 0x04414020 /dev/mem opened. Memory mapped at address 0xffff8c5d4000. Read at address 0x04414020 (0xffff8c5d4020): 0x80000030 root@j784s4-evm:~# devmem2 0x04414028 /dev/mem opened. Memory mapped at address 0xffff8e149000. Read at address 0x04414028 (0xffff8e149028): 0x0000111F root@j784s4-evm:~# devmem2 0x04414034 /dev/mem opened. Memory mapped at address 0xffff912c9000. Read at address 0x04414034 (0xffff912c9034): 0x00000000 root@j784s4-evm:~# devmem2 0x04414038 /dev/mem opened. Memory mapped at address 0xffffb6a83000. Read at address 0x04414038 (0xffffb6a83038): 0x00001F0F root@j784s4-evm:~# devmem2 0x04414084 /dev/mem opened. Memory mapped at address 0xffff91905000. Read at address 0x04414084 (0xffff91905084): 0x0B58044C root@j784s4-evm:~# devmem2 0x04414040 /dev/mem opened. Memory mapped at address 0xffff8b4fc000. Read at address 0x04414040 (0xffff8b4fc040): 0x00010000
关于串行器状态:
- 全局错误状态置为有效
- 未检测到 PCLK
你有什么想法,什么可能是问题?
我们在 TDA4VM 上使用26MHz 输入时钟。
此致、
Milena