工具/软件:
您好、
使用 HS 设备时、我的 MCU2_0显示屏如下所示。
root@j721e-evm:/opt/vision_apps# [MCU2_0] 4.983124 s: CIO: Init ... Done !!! [MCU2_0] 4.983199 s: ### CPU Frequency = 1000000000 Hz [MCU2_0] 4.983236 s: CPU is running FreeRTOS [MCU2_0] 4.983258 s: APP: Init ... !!! [MCU2_0] 4.983275 s: SCICLIENT: Init ... !!! [MCU2_0] 4.983500 s: SCICLIENT: DMSC FW version [10.0.8--v10.00.08 (Fiery Fox)] [MCU2_0] 4.983541 s: SCICLIENT: DMSC FW revision 0xa [MCU2_0] 4.983564 s: SCICLIENT: DMSC FW ABI revision 4.0 [MCU2_0] 4.983588 s: SCICLIENT: Init ... Done !!! [MCU2_0] 4.983611 s: UDMA: Init ... !!! [MCU2_0] 4.984876 s: UDMA: Init ... Done !!! [MCU2_0] 4.984945 s: MEM: Init ... !!! [MCU2_0] 4.984984 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ d9000000 of size 15728640 bytes !!! [MCU2_0] 4.985045 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!! [MCU2_0] 4.985092 s: MEM: Created heap (DDR_CACHE_WT_MEM, id=7, flags=0x00000000) @ d9f00000 of size 1048576 bytes !!! [MCU2_0] 4.985135 s: MEM: Init ... Done !!! [MCU2_0] 4.985154 s: ETHFW: Init ... !!! [MCU2_0] 5.244289 s: ETHFW: Warning: Using 6 random MAC address(es) [MCU2_0] 5.244413 s: ETHFW: Shared multicasts: [MCU2_0] 5.244460 s: ETHFW: 01:00:5e:00:00:01 [MCU2_0] 5.244492 s: ETHFW: 01:00:5e:00:00:fb [MCU2_0] 5.244522 s: ETHFW: 01:00:5e:00:00:fc [MCU2_0] 5.244550 s: ETHFW: 33:33:00:00:00:01 [MCU2_0] 5.244578 s: ETHFW: 33:33:ff:1d:92:c2 [MCU2_0] 5.244606 s: ETHFW: 01:80:c2:00:00:00 [MCU2_0] 5.244633 s: ETHFW: 01:80:c2:00:00:03 [MCU2_0] 5.244658 s: ETHFW: Reserved multicasts: [MCU2_0] 5.244687 s: ETHFW: 01:80:c2:00:00:0e [MCU2_0] 5.244716 s: ETHFW: 01:1b:19:00:00:00 [MCU2_0] 5.244759 s: ETHFW: CPSW recovery is not enabled [MCU2_0] 5.244978 s: EnetMcm: CPSW_9G on MAIN NAVSS [MCU2_0] 5.254356 s: Mdio_open: MDIO manual mode enabled [MCU2_0] 5.254426 s: [MCU2_0] 5.261681 s: [FATAL]: Core has Aborted!!! [MCU2_0] DFAR =0x0 DFSR =0x0 [MCU2_0] 5.261761 s: IFAR =0xe59ff018 IFSR =0xd [MCU2_0] 5.261790 s: CPSR =0x197 SP =0x0 [MCU2_0] 5.261809 s: LR =0x0 R0 =0x0 [MCU2_0] 5.261827 s: R1 =0x0 R2 =0x0 [MCU2_0] 5.261844 s: R3 =0x0 R4 =0x0 [MCU2_0] 5.261862 s: R5 =0x0 R6 =0x0 [MCU2_0] 5.261889 s: R7 =0x0 R8 =0x0 [MCU2_0] 5.261910 s: R9 =0x0 R10 =0x0 [MCU2_0] 5.261927 s: R11 =0x0 R12 =0x0
当我使用 GP 设备时、它实际上可以正常工作。
我无法找到问题的根源、您能帮助我看看问题可能在哪里吗?
此致、
Yang