工具/软件:
您好!
我尝试 在 CCS 12.8.1中将 Blackhawk USB560v2系统跟踪程序调试器(BH-USB-560v2)连接到 J7200 EVM。 CCS 报告的错误#-183。 我在下面附上了屏幕截图和日志。 我的 EVM 设置为无引导模式。 您能告诉我什么问题吗? 我预计该调试器开箱即用、因为 CCS 支持该调试器。
谢谢、
Charles
测试连接日志
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0] Execute the command: %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\rhlchmao\AppData\Local\TEXASI~1\ CCS\ccs1281\0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'bh560v2u.out'. Loaded FPGA Image: C:\ti\ccs1281\ccs\ccs_base\common\uscif\dtc_top.jbc The library build date was 'Sep 26 2024'. The library build time was '10:02:16'. The library package version is '20.0.0.3178'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-183' (0xffffff49). The title is 'SC_ERR_CTL_CBL_BREAK_FAR'. The explanation is: The controller has detected a cable break far-from itself. The user must connect the cable/pod to the target. [End: Blackhawk XDS560v2-USB System Trace Emulator_0]