工具/软件:
您好:
我更新了一些需要正确引导具有1GB DDR 的定制电路板的更改。 电路板正常启动、直到有用户空间。 但我发现下面附上了一些错误打印件。它是否影响板,如何克服这些错误打印件。
reboot: Restarting system
NOTICE: bl1_plat_arch_setup arch setup
NOTICE: Booting Trusted Firmware
NOTICE: BL1: v2.12.0(release):a36507324-dirty
NOTICE: BL1: Built : 05:35:22, Apr 29 2025
NOTICE: lpdd4_init <--
NOTICE: DDR ram size =40000000
NOTICE: bl1_platform_setup DDR init done
NOTICE: k3_bl1_handoff ENTERING WFI - end of bl1
NOTICE: BL31: v2.12.0(release):a36507324-dirty
NOTICE: BL31: Built : 05:35:22, Apr 29 2025
ERROR: Failed to get response (-19)
ERROR: Transfer send failed (-19)
ERROR: Agent 0 Protocol 0x10 Message 0x7: not supported
U-Boot SPL 2025.01-ge92ebf9f7bcb (Apr 28 2025 - 11:07:19 +0000)
SPL initial stack usage: 1744 bytes
Trying to boot from MMC2
ERROR: Agent 0 Protocol 0x10 Message 0x7: not supported
U-Boot 2025.01-ge92ebf9f7bcb (Apr 28 2025 - 11:07:19 +0000)
SoC: AM62LX SR1.0 HS-FS
Model: iG-RainboW-G69M-TI-AM62LX OSM
DRAM: 1 GiB
ERROR: Agent 0 Protocol 0x10 Message 0x7: not supported
Core: 59 devices, 27 uclasses, devicetree: separate
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Board Info:
BSP Version : iG-PRITZ-SC-01-R1.0-REL0.1-Linux6.12.13
SOM Version : iG-PRITZ-AP-01-R1.0
Net: ADIN1300 PHY detected at addr 4
Warning: ethernet@8000000port@1 MAC addresses don't match:
Address in ROM is 44:6b:1f:35:33:54
Address in environment is a0:cd:f3:77:ef:49
eth0: ethernet@8000000port@1 [PRIME]
Hit any key to stop autoboot: 0
错误:未能获得响应(-19)
错误:传输发送失败(-19)
错误:代理0协议0x10消息0x7:不支持
--此致、
Dheeraj k