This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA3XEVM:摄像头 CPI 端口

Guru**** 2466550 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1523331/tda3xevm-camera-cpi-port

器件型号:TDA3XEVM

工具/软件:

我将使用 TDA3定制板。

传感器当前连接到 CPI 端口。

数据是 RAW14位。

我将其设置如下、但出现了错误。

SYSTEM_DF_RAW16;
SYSTEM_VIFW_16BIT
SYSTEM_VIFM_SCH_CPI
[IPU1-0]      2.296346 s:  
[IPU1-0]      2.296376 s:  Entered chains_iss_Canlab_Display 
[IPU1-0]      2.297169 s:  ISSCAPTURE: Create in progress !!!
[IPU1-0]      2.347526 s:  UTILS: DMA: Allocated CH (TCC) = 48 (48)
[IPU1-0]      2.347648 s:  UTILS: DMA: 0 of 1: Allocated PaRAM = 48 (0x63304800)
[IPU1-0]      2.347861 s:  ISSCAPTURE: Create Done !!!
[IPU1-0]      2.348319 s:  DISPLAY: Create in progress !!!
[IPU1-0]      2.348624 s: dispcore/src/vpscore_dss.c @ Line 1137: 
[IPU1-0]      2.348685 s: Un supported data format 
[IPU1-0]      2.348776 s: dispdrv/src/vpsdrv_displayCore.c @ Line 304: 
[IPU1-0]      2.348837 s: Set DSS parameter failed
[IPU1-0]      2.348898 s:  Assertion @ Line: 459 in displayLink_drv.c: status==SYSTEM_LINK_STATUS_SOK : failed !!!
[IPU1-0]      2.349386 s:  Assertion @ Line: 459 in displayLink_drv.c: status==SYSTEM_LINK_STATUS_SOK : failed !!!
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Kim:

    但从下面的错误,它似乎你正在使用这个数据格式在显示屏中也... 请注意、显示屏不支持 RAW14数据格式、因此您需要将此格式转换为 YUV 或 RGB 等可视格式、然后才能在显示屏中使用。

    ispcore/vpscore_dss.c src @第1137行:

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好

    更改 info->dataFormat = SYSTEM_DF_YUV422I_UYVY;后
    、错误消失。

    但是、当使用"p"进行检查时、不会检测到帧捕获。

    由于定制电路板上没有 HDMI、因此 HDMI INIT 部分被注释掉。

    [IPU1-0]  ====================
    [IPU1-0]  Chains Run-time Menu
    [IPU1-0]  ====================
    [IPU1-0]  
    [IPU1-0]  0: Stop Chain
    [IPU1-0]  
    [IPU1-0]  
    [IPU1-0]  p: Print Performance Statistics 
    [IPU1-0]  
    [IPU1-0]  Enter Choice: 
    [IPU1-0]  
    [IPU1-0]     23.338772 s:  
    [IPU1-0]     23.338833 s:  CPU [IPU1-0 ] Statistics, 
    [IPU1-0]     23.338894 s:  ************************* 
    [IPU1-0]     23.338955 s:  
    [IPU1-0]     23.339016 s:  LOAD: CPU: 4.9% HWI: 0.5%, SWI:0.3%, Low Power: 1.7% 
    [IPU1-0]     23.339138 s:  
    [IPU1-0]     23.339291 s:  LOAD: TSK: GrpxSrc0            : 2.3% 
    [IPU1-0]     23.339382 s:  LOAD: TSK: STAT_COLL           : 1.3% 
    [IPU1-0]     23.339443 s:  LOAD: TSK: MISC                : 0.5% 
    [IPU1-0]     23.339535 s:  
    [IPU1-0]     23.339565 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1022 
    [IPU1-0]     23.339657 s:  
    [IPU1-0]     23.339687 s:  SYSTEM: Sempahores Objects,  140 of 1050 free 
    [IPU1-0]     23.339779 s:  SYSTEM: Task Objects      ,   13 of  100 free 
    [IPU1-0]     23.339870 s:  SYSTEM: Clock Objects     ,   97 of  100 free 
    [IPU1-0]     23.339962 s:  SYSTEM: Hwi Objects       ,   87 of  100 free 
    [IPU1-0]     23.340053 s:  
    [IPU1-0]     23.340084 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 257576 B (251 KB)
    [IPU1-0]     23.340236 s:  SYSTEM: Heap = SR_OCMC              @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
    [IPU1-0]     23.340389 s:  SYSTEM: Heap = SR_DDR_CACHED        @ 0x86103000, Total size = 369086464 B (351 MB), Free size = 361252864 B (344 MB)
    [IPU1-0]     23.340541 s:  SYSTEM: Heap = SR_DDR_NON_CACHED    @ 0xbfe00000, Total size = 916224 B (0 MB), Free size = 916224 B (0 MB)
    [IPU1-0]     23.340694 s:  
    [IPU1-0]     23.340846 s:  
    [IPU1-0]     23.340877 s:  UTILS_PRCM_STATS:  Current Temperature,
    [IPU1-0]     23.340938 s:  
    [IPU1-0]     23.340999 s:   Voltage Rail         ||   Curr Temp Min - Max   
    [IPU1-0]     23.341090 s:  --------------------------------------------------------- 
    [IPU1-0]     23.341212 s:     PMHAL_PRCM_VD_CORE ||     [69.600 , 70.  0]    
    [IPU1-0]     23.341304 s: 
    [IPU1-0]     23.341395 s:  
    [IPU1-0]     23.341426 s:  Statistics Collector,
    [IPU1-0]     23.341487 s:  
    [IPU1-0]     23.341517 s:        STATISTIC          Avg Data        Peak Data 
    [IPU1-0]     23.341609 s:        COLLECTOR          MB/s            MB/s      
    [IPU1-0]     23.341670 s:  -------------------------------------------------- 
    [IPU1-0]     23.341761 s:  SCI_EMIF_SYS         |    211.287049    274.163134
    [IPU1-0]     23.341883 s:  SCI_IPU              |     16.303181    159.249100
    [IPU1-0]     23.341975 s:  SCI_DSP1_MDMA        |      0.000000      0.000000
    [IPU1-0]     23.342066 s:  SCI_DSP2_MDMA        |      0.000000      0.000000
    [IPU1-0]     23.342188 s:  SCI_DSS              |    195.134971    261.819352
    [IPU1-0]     23.342280 s:  SCI_MMU              |      0.000000      0.000000
    [IPU1-0]     23.342371 s:  SCI_EDMA_TC0_RD      |      0.000000      0.000000
    [IPU1-0]     23.342463 s:  SCI_EDMA_TC0_WR      |      0.000000      0.000000
    [IPU1-0]     23.342585 s:  SCI_VIP_P1           |      0.000000      0.000000
    [IPU1-0]     23.342676 s:  SCI_VIP_P2           |      0.000000      0.000000
    [IPU1-0]     23.342890 s:  SCI_ISS_RT           |      0.000000      0.000000
    [IPU1-0]     23.342981 s:  SCI_ISS_NRT2         |      0.000000      0.000000
    [IPU1-0]     23.343073 s:  SCI_EVE_P1           |      0.000000      0.000000
    [IPU1-0]     23.343164 s:  SCI_EVE_P2           |      0.000000      0.000000
    [IPU1-0]     23.343286 s:  SCI_GMAC_SW          |      0.000000      0.000000
    [IPU1-0]     23.343378 s:  SCI_ISS_NRT1         |      0.000000      0.000000
    [IPU1-0]     23.343469 s:  SCI_DSP2_CFG         |      0.000000      0.000000
    [IPU1-0]     23.343561 s:  SCI_DSP2_EDMA        |      0.000000      0.000000
    [IPU1-0]     23.343652 s:  SCI_OCMC_RAM         |      0.000000      0.000000
    [IPU1-0]     23.343744 s:  SCI_DSP1_CFG         |      0.000000      0.000000
    [IPU1-0]     23.343866 s:  SCI_DSP1_EDMA        |      0.000000      0.000000
    [IPU1-0]     23.343957 s:  SCI_GPMC             |      0.000000      0.000000
    [IPU1-0]     23.344049 s:  SCI_MCASP            |      0.000000      0.000000
    [IPU1-0]     23.344171 s:  SCI_EDMA_TC1_RD      |      0.000000      0.000000
    [IPU1-0]     23.344262 s:  SCI_EDMA_TC1_WR      |      0.000000      0.000000
    [IPU1-0]     23.443786 s:  
    [IPU1-0]     23.443847 s:  
    [IPU1-0]     23.443939 s:  
    [IPU1-0]     23.443969 s:  ### CPU [IPU1-0], LinkID [ 87],
    [IPU1-0]     23.444061 s:  
    [IPU1-0]     23.444091 s:  [ ISSCAPTURE ] Link Statistics,
    [IPU1-0]     23.444213 s:  ******************************
    [IPU1-0]     23.444274 s:  
    [IPU1-0]     23.444305 s:  Elapsed time       = 20867 msec
    [IPU1-0]     23.444366 s:  
    [IPU1-0]     23.444396 s:  
    [IPU1-0]     23.444458 s:  Input Statistics,
    [IPU1-0]     23.444488 s:  
    [IPU1-0]     23.444519 s:  CH | In Recv | In Drop | In User Drop | In Process 
    [IPU1-0]     23.444610 s:     | FPS     | FPS     | FPS          | FPS        
    [IPU1-0]     23.444671 s:  -------------------------------------------------- 
    [IPU1-0]     23.444763 s:  
    [IPU1-0]     23.444824 s:  Output Statistics,
    [IPU1-0]     23.444854 s:  
    [IPU1-0]     23.444885 s:  CH | Out | Out     | Out Drop | Out User Drop 
    [IPU1-0]     23.444976 s:     | ID  | FPS     | FPS      | FPS           
    [IPU1-0]     23.445037 s:  --------------------------------------------- 
    [IPU1-0]     23.445129 s:  
    [IPU1-0]     23.445159 s:  [ ISSCAPTURE ] LATENCY,
    [IPU1-0]     23.445220 s:  ********************
    [IPU1-0]     23.445251 s:  
    [IPU1-0]     23.445373 s:  
    [IPU1-0]     23.445403 s:  ### CPU [IPU1-0], LinkID [ 77],
    [IPU1-0]     23.445464 s:  
    [IPU1-0]     23.445495 s:  [ DISPLAY ] Link Statistics,
    [IPU1-0]     23.445556 s:  ******************************
    [IPU1-0]     23.445617 s:  
    [IPU1-0]     23.445647 s:  Elapsed time       = 20867 msec
    [IPU1-0]     23.445739 s:  
    [IPU1-0]     23.445769 s:  
    [IPU1-0]     23.445800 s:  Input Statistics,
    [IPU1-0]     23.445861 s:  
    [IPU1-0]     23.445891 s:  CH | In Recv | In Drop | In User Drop | In Process 
    [IPU1-0]     23.445983 s:     | FPS     | FPS     | FPS          | FPS        
    [IPU1-0]     23.446044 s:  -------------------------------------------------- 
    [IPU1-0]     23.446105 s:  
    [IPU1-0]     23.446166 s:  Output Statistics,
    [IPU1-0]     23.446196 s:  
    [IPU1-0]     23.446227 s:  CH | Out | Out     | Out Drop | Out User Drop 
    [IPU1-0]     23.446318 s:     | ID  | FPS     | FPS      | FPS           
    [IPU1-0]     23.446379 s:  --------------------------------------------- 
    [IPU1-0]     23.446471 s:  
    [IPU1-0]     23.446501 s:  [ DISPLAY ] LATENCY,
    [IPU1-0]     23.446562 s:  ********************
    [IPU1-0]     23.446593 s:  
    [IPU1-0]     23.446623 s:  Display UnderFlow Count = 0
    [IPU1-0]     23.446684 s:  
    [IPU1-0]     23.446745 s:  CPU [  IPU1-0], LinkID [ 23], Link Statistics not available !
    [IPU1-0]     23.446898 s:  
    [IPU1-0]     23.446928 s:  ### CPU [IPU1-0], LinkID [ 78],
    [IPU1-0]     23.447020 s:  
    [IPU1-0]     23.447050 s:  [ DISPLAY ] Link Statistics,
    [IPU1-0]     23.447111 s:  ******************************
    [IPU1-0]     23.447172 s:  
    [IPU1-0]     23.447203 s:  Elapsed time       = 18933 msec
    [IPU1-0]     23.447264 s:  
    [IPU1-0]     23.447294 s:  Driver/Notify Cb   =  60.21 fps
    [IPU1-0]     23.447386 s:  
    [IPU1-0]     23.447416 s:  Input Statistics,
    [IPU1-0]     23.447477 s:  
    [IPU1-0]     23.447508 s:  CH | In Recv | In Drop | In User Drop | In Process 
    [IPU1-0]     23.447569 s:     | FPS     | FPS     | FPS          | FPS        
    [IPU1-0]     23.447660 s:  -------------------------------------------------- 
    [IPU1-0]     23.447721 s:   0 |   0. 5      0. 0      0. 0           0. 5 
    [IPU1-0]     23.447965 s:  
    [IPU1-0]     23.447996 s:  [ DISPLAY ] LATENCY,
    [IPU1-0]     23.448057 s:  ********************
    [IPU1-0]     23.448118 s:  Local Link Latency     : Avg =     31 us, Min =     31 us, Max =     31 us, 
    [IPU1-0]     23.448209 s:  Source to Link Latency : Avg = 482706 us, Min = 482706 us, Max = 482706 us, 
    [IPU1-0]     23.448331 s:  
    [IPU1-0]     23.448362 s:  Display UnderFlow Count = 0
    [IPU1-0]     23.448423 s:  
    [IPU1-0]     23.947874 s: 
    [IPU1-0]  
    [IPU1-0]  ====================
    [IPU1-0]  Chains Run-time Menu
    [IPU1-0]  ====================
    [IPU1-0]  
    [IPU1-0]  0: Stop Chain
    [IPU1-0]  
    [IPU1-0]  
    [IPU1-0]  p: Print Performance Statistics 
    [IPU1-0]  
    [IPU1-0]  Enter Choice: 
    [IPU1-0]  
    
    
    

    此致、

    Kim

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我需要修改哪些寄存器来更改 CPI 端口上 vsync 和 HSYNC 的极性?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    修改相关零件后、没有发生错误、且消息正常接收。