Other Parts Discussed in Thread: AM625, SK-AM62-LP
主题中讨论的其他器件: SK-AM62-LP
工具/软件:
我们有一个使用 AM6232的定制电路板、RMII 模式下的以太网 PHY 为 Micrel XZ8041。
我已 从 ti-u-boot-2024.04创建了所需的3个文件、并将其复制到 DHCP/TFP 服务器、该服务器通过 USB 以太网端口(即专用端口)连接到 AM62。
在加电时、我可以看到 tiboot.bin 的初始 TFTP 工作并且 SPL 会执行。
尽管看到 PHY 被检测到并且链路有效、但我看不到 BOOTP 广播的任何 TX 输出。
您是否可以建议我查看一些区域以尝试诊断 TX 为什么没有将其发送到以太网输出?
已附加引导日志。
谢谢你。
U-Boot SPL 2024.04-00002-gbaa288e477f-dirty (Mar 27 2025 - 09:38:30 +0000)SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')SPL initial stack usage: 13392 bytesTrying to boot from eth deviceethernet@8000000port@1 connected to Micrel KSZ804 mode rmiieth0: ethernet@8000000port@1ethernet@8000000port@1 Waiting for PHY auto negotiation to complete..... donelink up on port 1, speed 100, full duplexBOOTP broadcast 1BOOTP broadcast 2BOOTP broadcast 3BOOTP broadcast 4BOOTP broadcast 5BOOTP broadcast 6BOOTP broadcast 7BOOTP broadcast 8BOOTP broadcast 9BOOTP broadcast 10BOOTP broadcast 11BOOTP broadcast 12BOOTP broadcast 13BOOTP broadcast 14BOOTP broadcast 15BOOTP broadcast 16BOOTP broadcast 17
Retry time exceeded; starting againudma_stop_mem2dev: peer not stopped TIMEOUT !Problem booting with BOOTPSPL: failed to boot from all boot devices### ERROR ### Please RESET the board ###