This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] J721EXSOMXEVM:勘误表 i2086 TI XIO2001单功能 PCI Express 至 PCI 转换桥接器问题

Guru**** 2466940 points
Other Parts Discussed in Thread: XIO2001, SK-TDA4VM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1523570/j721exsomxevm-errata-i2086-issue-with-ti-xio2001-single-function-pci-express-to-pci-translation-bridge

器件型号:J721EXSOMXEVM
主题中讨论的其他器件:XIO2001SK-TDA4VM

工具/软件:

您好:

我基于 J721e SoC 的客户电路板使用包含 德州仪器(TI) XIO2001 PCI Express 转 PCI 桥接器[104C:8240]的 PCIe 器件。
但是、正如  关于 PCIe 开关和多功能设备勘误表 i2086的常见问题解答中所报告的、PCI 枚举期间内核崩溃:

[    0.367547] j721e-pcie-host 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[    0.367563] j721e-pcie-host 2910000.pcie: Parsing ranges property...
[    0.367575] j721e-pcie-host 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
[    0.367588] j721e-pcie-host 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
[    0.367593] j721e-pcie-host 2910000.pcie: Parsing dma-ranges property...
[    0.367599] j721e-pcie-host 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    0.469891] j721e-pcie-host 2910000.pcie: Link up
[    0.493902] j721e-pcie-host 2910000.pcie: LINK DOWN!
[    0.594001] j721e-pcie-host 2910000.pcie: Link up
[    0.594091] j721e-pcie-host 2910000.pcie: PCI host bridge to bus 0000:00
[    0.594096] pci_bus 0000:00: root bus resource [bus 00-ff]
[    0.594101] pci_bus 0000:00: root bus resource [io  0x0000-0xffff] (bus address [0x18001000-0x18010fff])
[    0.594104] pci_bus 0000:00: root bus resource [mem 0x18011000-0x1fffffff]
[    0.594108] pci_bus 0000:00: scanning bus
[    0.594134] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[    0.594138] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    0.594210] pci 0000:00:00.0: supports D1
[    0.594213] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[    0.594218] pci 0000:00:00.0: PME# disabled
[    0.594358] pci 0000:00:00.0: vgaarb: pci_notify
[    0.595863] pci_bus 0000:00: fixups for bus
[    0.595866] pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 0
[    0.595870] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    0.595876] pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1
[    0.595923] pci_bus 0000:01: scanning bus
[    0.595972] pci 0000:01:00.0: [104c:8240] type 01 class 0x060400
[    0.596216] pci 0000:01:00.0: supports D1 D2
[    0.596372] pci 0000:01:00.0: vgaarb: pci_notify
[    0.620418] j721e-pcie-host 2910000.pcie: LINK DOWN!
[    1.766328] pci_bus 0000:01: fixups for bus
[    1.766335] pci 0000:01:00.0: scanning [bus 00-00] behind bridge, pass 0
[    1.766339] pci 0000:01:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    1.766357] pci 0000:01:00.0: scanning [bus 00-00] behind bridge, pass 1
[    1.766472] pci_bus 0000:02: extended config space not accessible
[    1.766504] pci_bus 0000:02: scanning bus
[    1.766526] pci 0000:02:00.0: [15cf:0000] type 00 class 0xff0000
[    1.766567] pci 0000:02:00.0: reg 0x10: [mem 0x00000000-0x0000ffff]
[    1.766761] pci 0000:02:00.0: vgaarb: pci_notify
[    1.766787] SError Interrupt on CPU1, code 0x00000000bf000000 -- SError
[    1.766792] CPU: 1 PID: 9 Comm: kworker/u4:0 Not tainted 6.1.119-rt45 #78
[    1.766796] Hardware name: BeagleBoard.org BeagleBone AI-64 (DT)

由于此问题特定于 J721e SoC、因此我可以使用 TI SK-TDA4VM 和 BeagleBone-AI64板重现该问题。

注意:与常见问题解答中的日志不同、我在每个电路板上都注意到链路接通->下->上->下序列:

[    0.469891] j721e-pcie-host 2910000.pcie: Link up
[    0.493902] j721e-pcie-host 2910000.pcie: LINK DOWN!
[    0.594001] j721e-pcie-host 2910000.pcie: Link up
...
[    0.620418] j721e-pcie-host 2910000.pcie: LINK DOWN!

PCIe 设备似乎不支持 PCIe ARI 转发功能(因此常见问题解答解决方法1不适用)。

 常见问题解答变通办法#2似乎不适用于我的用例、XIO2001是一个单功能 PCI Express 至 PCI 转换桥接器(我不确定如何创建5个 虚拟函数)

因此、唯一剩下的权变措施3是修补内核以忽略系统中止并恢复正常运行。

实际上、内核在 PCI 枚举期间不再崩溃、但未检测到设备(由于链路断开?)
我必须手动重新扫描 PCIe 总线以检测 CIFX PCI/PCIe [15CF:0000]

# lspci 
00:00.0 PCI bridge: Texas Instruments Device b00d
01:00.0 PCI bridge: Texas Instruments XIO2001 PCI Express-to-PCI Bridge
 
# echo 1 > /sys/class/pci_bus/0000:00/rescan
[   37.644278] pci 0000:01:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[   37.644410] pci_bus 0000:02: extended config space not accessible
[   37.646080] pci_bus 0000:02: busn_res: can not insert [bus 02-01] under [bus 01] (conflicts with (null) [bus 01])
[   37.646119] pci 0000:02:00.0: [15cf:0000] type 00 class 0xff0000 conventional PCI endpoint
[   37.646243] pci 0000:02:00.0: BAR 0 [mem 0x00000000-0x0000ffff]
[   37.651341] pci_bus 0000:02: busn_res: [bus 02-01] end is updated to 02
[   37.651347] pci_bus 0000:02: busn_res: can not insert [bus 02] under [bus 01] (conflicts with (null) [bus 01])
[   37.651356] pci 0000:01:00.0: devices behind bridge are unusable because [bus 02] cannot be assigned for them
[   37.651369] pcieport 0000:00:00.0: bridge has subordinate 01 but max busn 02
[   37.651402] pcieport 0000:00:00.0: bridge window [mem 0x4100200000-0x41002fffff]: assigned
[   37.651407] pci 0000:01:00.0: bridge window [mem 0x4100200000-0x41002fffff]: assigned
[   37.651411] pci 0000:02:00.0: BAR 0 [mem 0x4100200000-0x410020ffff]: assigned
[   37.651422] pci 0000:01:00.0: PCI bridge to [bus 02]
[   37.651651] pci 0000:01:00.0:   bridge window [mem 0x4100200000-0x41002fffff]
 
# lspci 
00:00.0 PCI bridge: Texas Instruments Device b00d
01:00.0 PCI bridge: Texas Instruments XIO2001 PCI Express-to-PCI Bridge
02:00.0 Unassigned class [ff00]: Hilscher Gesellschaft für Systemautomation mbH CIFX PCI/PCIe


我在 SK-TDA4VM 和 BeagleboneAI64上使用了几个 Yocto kirkstone 的内核版本 TI 6.1、scarthgap 的 TI 6.12和 vanilla 6.15+内核(主器件)。

解决此问题的进展是否在上游?

此致、
罗曼语

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Romain:

    [引述 userid="333284" url="~/support/processors-group/processors/f/processors-forum/1523570/j721exsomxevm-errata-i2086-issue-with-ti-xio2001-single-function-pci-express-to-pci-translation-bridge

    解决此问题的进展是否在上游?

    [/报价]

    目前、没有 常见问题解答中的权变措施是当前可用的解决方法。 PCIe 开关在勘误表 i2086方面尤其存在问题、因为即使创建了虚拟函数、常见问题解答中的权变措施2也不起作用。

    可用的解决方法 是忽略错误的解决方法#3。 在本例中、还有一个在引导时运行的附加脚本、用于重新扫描 PCIe 总线。  

    此致、

    Takuma

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、 Takuma、

    感谢您的回复、感谢您的常见问题解答页面!

    您是否有关于此问题的更多详细信息、为什么它特定于 J721e SoC、而其他 K3 SoC 型号不存在该问题?

    此致、
    罗曼语

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Romain:

    J721e 是第一个发布的 J7 SoC、具有该问题。 其他 K3 SoC 稍后发布、因此我们在器件中进行了修复。

    该问题是 J721e 如何处理来自 PCIe 器件的 UR (不受支持的请求)响应造成的。 J721e 将其视为不可恢复的总线错误、但事实证明可以为 PCIe 器件的正常运行生成 UR 响应。 具体而言、当探测连接了未知数量 PCIe 器件的器件(包括具有多个物理功能(理论上最多为6个、但可能在1到6之间)或 PCIe 开关(理论上、最多可以连接256个不同器件)的总线时、使用 UR 响应来指示某个器件未填充特定的 PCIe 地址。 因此、权变措施本质上是不生成 UR 响应的方法、对于权变措施3、假设总线错误是由 PCIe 的 UR 响应引起的、则忽略总线错误。

    此致、

    Takuma