This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRA821U:J7200-EVM 上的 QuadPhy 问题

Guru**** 2475290 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1534691/dra821u-issues-with-the-quadphy-on-the-j7200-evm

器件型号:DRA821U

工具/软件:

您好:

这是以下主题的后续内容:
DRA821U:如何通过当前 SDK(处理器论坛-处理器 — TI E2E 支持论坛)在 ethfw 中将多个仅 MAC 端口映射到 A72

让 J7200-EVM 上的 QuadPhy 正常工作时仍存在问题。 收到补丁后、我使用最新的 Linux SDK 和 ethfw 构建了一个全新的版本。 我还停用了 gPTP、并按照上述线程中的建议更改了 MAC 地址。 端口配置未更改、因此没有其他仅 MAC 端口。

我可以通过 CPSW2G 端口 ping 所有静态 IP(分配给 eth0、eth1 和 eth2)、但连接到 CPSW5G 上的任何 MAC 端口时都没有响应。

root@j7200-evm:~# dmesg | grep eth
[    0.000000] psci: probing for conduit method from DT.
[    0.814966] optee: probing for conduit method.
[    1.270545] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    1.283402] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    1.290612] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    1.300962] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[    3.062533] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    3.075399] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    3.082609] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    3.092924] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[    3.109044] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    3.862713] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    3.941210] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    7.929338] virtio_rpmsg_bus virtio1: creating channel ti.ethfw.ethdevice addr 0x22
[    8.234417] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[    8.289677] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[    8.708399] ti_cpsw_proxy_client virtio1.ti.ethfw.ethdevice.-1.34: 1 Virtual Switch Port(s), 1 Virtual MAC Only Port(s)
[    8.720610] ti_cpsw_proxy_client virtio1.ti.ethfw.ethdevice.-1.34: Virt Port: 0, Type: Switch Port, Iface: eth1, Num TX: 2, Num RX: 1, Token: 0
[    8.735769] ti_cpsw_proxy_client virtio1.ti.ethfw.ethdevice.-1.34: Virt Port: 4, Type: MAC Port, Iface: eth2, Num TX: 1, Num RX: 1, Token: 400
[    9.060691] ti_cpsw_proxy_client virtio1.ti.ethfw.ethdevice.-1.34: started port 4 on interface eth2
[    9.190333] ti_cpsw_proxy_client virtio1.ti.ethfw.ethdevice.-1.34: started port 0 on interface eth1
[   85.189291] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 10Mbps/Full - flow control off

root@j7200-evm:~# cat /sys/kernel/debug/remoteproc/remoteproc1/trace0
ETHFW: Detected boards: QSGMII
=======================================================
            CPSW Ethernet Firmware
=======================================================
ETHFW: Warning: Using 6 random MAC address(es)
EnetMcm: CPSW_5G on MAIN NAVSS
Mdio_open: MDIO manual mode enabled
PHY 16 is alive
PHY 17 is alive
PHY 18 is alive
PHY 19 is alive
EnetPhy_bindDriver: PHY 16: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
EnetPhy_bindDriver: PHY 17: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
EnetPhy_bindDriver: PHY 18: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
EnetPhy_bindDriver: PHY 19: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
ETHFW: Shared multicasts:
ETHFW:   01:00:5e:00:00:01
ETHFW:   01:00:5e:00:00:fb
ETHFW:   01:00:5e:00:00:fc
ETHFW:   33:33:00:00:00:01
ETHFW:   33:33:ff:1d:92:c2
ETHFW:   01:80:c2:00:00:00
ETHFW:   01:80:c2:00:00:03
ETHFW: Reserved multicasts:
ETHFW:   01:80:c1:00:00:0e
ETHFW:   01:1b:19:00:00:00
ETHFW: CPSW recovery is not enabled
ETHFW: VLAN 1024 member=0xd virtMember=0x7 regMcastFlood=0xd unregMcastFlood=0xd untag=0x0
ETHFW: 1 VLAN entries added in ALE table

ETHFW Version   : 0.05.00
ETHFW Build Date: Jul  1, 2025
ETHFW Build Time: 15:50:55
ETHFW Commit SHA:

Starting lwIP, local interface IP is dhcp-enabled
ETHFW: Host MAC address: 70:1e:76:40:0e:bc
[LWIPIF_LWIP] Enet LLD netif initialized successfully
[LWIPIF_LWIP_IC] Interface started successfully
[LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[LWIPIF_LWIP_IC] Interface started successfully
[LWIPIF_LWIP_IC] NETIF INIT SUCCESS
Added interface 'br3', IP is 0.0.0.0
ETHFW: Virtual port configuration:
ETHFW: CpswProxyServer: initialization completed (core: mcu2_0)
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
EnetPhy_findCommonNwayCaps: PHY 19: no common caps found
CpswMacPort_checkSgmiiStatus: MAC 4: SGMII link parter config port: link up: 1-Gbps Full-Duplex
Cpsw_handleLinkUp: Port 4: Link up: 1-Gbps Full-Duplex
ETHFW: Announce Endpoint Service to HLOS
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
ETHFW: VIRT_PORT_INFO | C2S | core=0 endpt=1025
ETHFW: VIRT_PORT_INFO | S2C | switchPortMask=1 macPortMask=10
ETHFW: ATTACH | C2S | core=0 endpt=1025 virtPort=0
ETHFW: ATTACH | S2C | token=0 rxMtu=1522 features=3
ETHFW: ATTACH | C2S | core=0 endpt=1025 virtPort=4
ETHFW: ATTACH | S2C | token=400 rxMtu=1522 features=1
ETHFW: ALLOC_RX | C2S | core=0 endpt=1025 token=0
ETHFW: ALLOC_RX | S2C | flow=84,0 rxPsil=0x4a00 status=0
ETHFW: ALLOC_TX | C2S | core=0 endpt=1025 token=0
ETHFW: ALLOC_TX | S2C | txPsil=0xca04 status=0
ETHFW: ALLOC_TX | C2S | core=0 endpt=1025 token=0
ETHFW: ALLOC_TX | S2C | txPsil=0xca07 status=0
ETHFW: ALLOC_MAC | C2S | core=0 endpt=1025 token=0
ETHFW: ALLOC_MAC | S2C | macAddr=70:c8:e3:0a:f5:43 status=0
ETHFW: ALLOC_RX | C2S | core=0 endpt=1025 token=400
ETHFW: ALLOC_RX | S2C | flow=84,1 rxPsil=0x4a00 status=0
ETHFW: ALLOC_TX | C2S | core=0 endpt=1025 token=400
ETHFW: ALLOC_TX | S2C | txPsil=0xca03 status=0
ETHFW: ALLOC_MAC | C2S | core=0 endpt=1025 token=400
ETHFW: ALLOC_MAC | S2C | macAddr=70:f9:17:0c:b6:e0 status=0
ETHFW: REGISTER_MAC | C2S | core=0 endpt=1025 token=400 macAdd=70:f9:17:0c:b6:e0 flowIdx=84,1
ETHFW: REGISTER_MAC | S2C | status=0
ETHFW: REGISTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=70:c8:e3:0a:f5:43 flowIdx=84,0
Cpsw_ioctlInternal: Registered MAC address (ALE entry=8, policer entry=1)
ETHFW: REGISTER_MAC | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=33:33:00:00:00:01 vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=01:00:5e:00:00:01 vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=33:33:ff:0a:f5:43 vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=01:80:c2:00:00:00 vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=01:80:c2:00:00:03 vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=01:80:c2:00:00:0e vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=33:33:00:00:00:fb vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
ETHFW: REGISTER_IPv4 | C2S | core=0 endpt=1025 token=0 ipAddr=192.168.100.171 macAdd=70:c8:e3:0a:f5:43
ETHFW:
 SNo.      MAC Address        VLAN     IP Address
ETHFW: ------  -------------------  ------  -----------------
ETHFW:     1    70:c8:e3:0a:f5:43       0    192.168.100.171
ETHFW: REGISTER_IPv4 | S2C | status=0
ETHFW: ADD_FILTER_MAC | C2S | core=0 endpt=1025 token=0 macAdd=01:00:5e:00:00:fb vlanId=65535 flowIdx=84,0
ETHFW: ADD_FILTER_MAC | S2C | status=0
Cpsw_handleLinkDown: Port 4: Link down
EnetPhy_findCommonNwayCaps: PHY 17: no common caps found
EnetPhy_findCommonNwayCaps: PHY 17: no common caps found
EnetPhy_findCommonNwayCaps: PHY 17: no common caps found
EnetPhy_findCommonNwayCaps: PHY 17: no common caps found

似乎出现错误消息“EnetPhy_findCommonNwayCaps:PHY 1x:No comon cap found“。 这可能是什么原因?

我还能做什么才能使其正常工作?

提前感谢!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    似乎出现错误消息“EnetPhy_findCommonNwayCaps:PHY 1x:未找到常用大写字母“。 这可能是什么原因?

    它将在 PHY 复位和协商过程中、PHY 状态机不打印常见的 Nway Cap。

    我可以看到 MAC 端口 4 与 1Gbps 链接在一起。
    CpswMacPort_checkSgmiiStatus:Mac 4:SGMII 链路参数配置端口:链路接通:1Gbps 全双工
    Cpsw_handleLinkUp:端口 4:链路接通:1Gbps 全双工

    默认情况下、MAC 端口 4 映射到 RTOS 客户端、作为仅 MAC 端口。 只有 MCU2_1 客户端才能通过 MAC 端口 4 进行通信。

    要与 eth1 通信、请确保从 MAC 端口 2/3 建立链路;同样、要 与 eth2 通信、请确保从 MAC 端口 1 建立链路。

    此致、
    Sudheer

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    感谢您的信息!

    至于日志,我尝试了各种不同的排列(从各种 MAC 端口 ping 所有不同的 eth 接口),但它不起作用。 另一方面、我尝试了本地 Linux 驱动程序、所有的 MAC 端口都开箱即用。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    至于日志、我尝试了各种不同的排列(ping 来自各种 MAC 端口的所有不同的 eth 接口)、但它不起作用。 另一方面、我尝试了本地 Linux 驱动程序、所有的 MAC 端口都开箱即用。  [/报价]

    ETHFW 应用程序开箱即用 TI SDK 应使用默认端口映射。

    我可以 从 Linux 虚拟交换机端口接口看到上述 192.168.100.171 的 IP 注册。  

    您能否确认、您对 ETHFW 应用程序进行了任何更改?  

    请使用默认 TI 配置检查一次。

    此外、 请确保 在 ETHFW 映射到 MCU2_0 内核时、本机 Linux 驱动程序启用 overlay。

    此致、
    Sudheer

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    ETHFW 应用程序开箱即用 TI SDK 应使用默认端口映射。

    我 PROCESSOR-SDK-LINUX-RT  使用最新版本  10.01.08.01 安装了 USB-J7200、并将预构建的二进制文件加载到 SD 卡上。 未进行任何更改。 我通过 Linux 命令行(例如 192.168.100.171)为接口分配了静态 IP 、但无法获得任何 ping。

    作为下一步。 我从 Yocto 环境获取了 Yocto 环境、并使用应用的补丁从 SDK 构建了一个映像(请参阅其他线程;当然也是关于 ethfw 的线程)。 我还停用了 gPTP 并按照另一个线程中的建议更改了 MAC 地址。 在这张图像中、我也无法获得任何 ping。

    另外、 确保 当 ETHFW 映射到 MCU2_0 内核时、不应用本机 Linux 驱动程序启用覆盖。

    不应用覆盖。

    我非常确定可以排除硬件设置问题、因为我可以通过 CPSW2G 上的 MAC 端口 ping 所有以太网接口。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    我已经按默认配置原样使用 TI SDK 进行了测试。
    用于测试 ETHFW 客户端网络的 SDK 如下所示。



    通过 CPSW 端口 2(交换机端口接口)将测试 PC 网络电缆连接到 EVM。  请  在下面找到从虚拟交换机端口接口 (eth1) 到测试 PC 的 ping 日志。


    QSGMII 的默认端口映射如下。
    https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-j784s4/latest/exports/docs/ethfw/docs/user_guide/ethfw_c_ug_top.html#ethfw_depend_evm_quadport_j7200


    已通过 Linux 上的仅虚拟 MAC 端口接口测试 MAC 端口 1 以测试 PC。 请参阅下面的 ping 日志。


    此致、
    Sudheer