主题: DRA821 中讨论的其他器件
工具/软件:
尊敬的 TI:
NOTICE: bl1_plat_arch_setup arch setup NOTICE: Booting Trusted Firmware NOTICE: BL1: v2.12.0(release):11.00.15-1-g2ae701def-dirty NOTICE: BL1: Built : 08:31:01, Jul 23 2025 NOTICE: BL1: dram_class: 10 NOTICE: lpddr4: post start - PI training status=0x29c02000 NOTICE: bl1_platform_setup DDR init done NOTICE: k3_bl1_handoff ENTERING WFI - end of bl1 NOTICE: bl1_plat_arch_setup arch setup NOTICE: Booting Trusted Firmware NOTICE: BL1: v2.12.0(release):11.00.15-1-g2ae701def-dirty NOTICE: BL1: Built : 08:31:01, Jul 23 2025 NOTICE: BL1: dram_class: 10 NOTICE: lpddr4: start failed status = 0x5 NOTICE: bl1_platform_setup DDR init failed