This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:使用 TDA4's CPSW9G、RGMII 连接到 PHY DP83TG720 链路接通、但 CAN't ping

Guru**** 2585275 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1560261/tda4vm-using-tda4-s-cpsw9g-rgmii-connecting-to-phy-dp83tg720-link-up-but-can-t-ping

器件型号:TDA4VM


工具/软件:

您好:

使用 TDA4 的 CPSW9G、port5-port8、其中 SGMII 连接到 phy 并成功 ping、port3、同时 RGMII 连接到 phy 芯片链路 、但我们无法 ping

SDK-10.01

1. UBoot

 2. Linux dts  k3-j721e-common-proc-board.dts

	rgmii3_default_pins: rgmii3-default-pins {
	pinctrl-single,pins = <
		J721E_IOPAD(0xb0, PIN_INPUT, 4) /* (AF28) PRG0_PRU0_GPO0.RGMII3_RD0 */
		J721E_IOPAD(0xb4, PIN_INPUT, 4) /* (AE28) PRG0_PRU0_GPO1.RGMII3_RD1 */
		J721E_IOPAD(0xb8, PIN_INPUT, 4) /* (AE27) PRG0_PRU0_GPO2.RGMII3_RD2 */
		J721E_IOPAD(0xbc, PIN_INPUT, 4) /* (AD26) PRG0_PRU0_GPO3.RGMII3_RD3 */
		J721E_IOPAD(0xc8, PIN_INPUT, 4) /* (AE26) PRG0_PRU0_GPO6.RGMII3_RXC */
		J721E_IOPAD(0xc0, PIN_INPUT, 4) /* (AD25) PRG0_PRU0_GPO4.RGMII3_RX_CTL */
		J721E_IOPAD(0xdc, PIN_OUTPUT, 4) /* (AJ28) PRG0_PRU0_GPO11.RGMII3_TD0 */
		J721E_IOPAD(0xe0, PIN_OUTPUT, 4) /* (AH27) PRG0_PRU0_GPO12.RGMII3_TD1 */
		J721E_IOPAD(0xe4, PIN_OUTPUT, 4) /* (AH29) PRG0_PRU0_GPO13.RGMII3_TD2 */
		J721E_IOPAD(0xe8, PIN_OUTPUT, 4) /* (AG28) PRG0_PRU0_GPO14.RGMII3_TD3 */
		J721E_IOPAD(0xf0, PIN_OUTPUT, 4) /* (AH28) PRG0_PRU0_GPO16.RGMII3_TXC */
		J721E_IOPAD(0xec, PIN_OUTPUT, 4) /* (AG27) PRG0_PRU0_GPO15.RGMII3_TX_CTL */
	>;
};



&cpsw0 {
	status = "okay";
	pinctrl-names = "default";
    pinctrl-0 = <&rgmii3_default_pins>;
};
&cpsw0_port1 {
	status = "disabled";
};

&cpsw0_port2 {
	status = "okay";
	phy-handle = <&cpsw9g_phy0>;
	phy-mode = "sgmii";
	mac-address = [00 00 00 00 00 00];
	phys = <&cpsw0_phy_gmii_sel 2>,<&serdes0_sgmii_link>;
	//phy-names = "portmode", "serdes-phy";
	phy-names = "portmode", "serdes";
};

&cpsw0_port3 {
	status = "okay";
	phy-handle = <&cpsw9g_phy13>;
	phy-mode = "rgmii-rxid";
	mac-address = [00 00 00 00 00 00];
	phys = <&cpsw0_phy_gmii_sel 3>;
};

&cpsw0_port4 {
	status = "disabled";
};

&cpsw0_port5 {
	status = "okay";
	phy-handle = <&cpsw9g_phy1>;
	phy-mode = "sgmii";
	mac-address = [00 00 00 00 00 00];
	phys = <&cpsw0_phy_gmii_sel 5>,<&serdes4_sgmii_link>;
    // phy-names = "portmode", "serdes-phy";
	phy-names = "portmode", "serdes";
	 
};

&cpsw0_port6 {
	status = "okay";
	phy-handle = <&cpsw9g_phy2>;
	phy-mode = "sgmii";
	mac-address = [00 00 00 00 00 00];
	phys = <&cpsw0_phy_gmii_sel 6>;
	//phy-names = "portmode", "serdes-phy";
	phy-names = "portmode", "serdes";
	
};

&cpsw0_port7 {
	status = "okay";
	phy-handle = <&cpsw9g_phy3>;
	phy-mode = "sgmii";
	mac-address = [00 00 00 00 00 00];
	phys = <&cpsw0_phy_gmii_sel 7>;
	//phy-names = "portmode", "serdes-phy";
	phy-names = "portmode", "serdes";
	
};

&cpsw0_port8 {
	status = "okay";
	phy-handle = <&cpsw9g_phy4>;
	phy-mode = "sgmii";
	mac-address = [00 00 00 00 00 00];
	phys = <&cpsw0_phy_gmii_sel 8>;
	//phy-names = "portmode", "serdes-phy";
	phy-names = "portmode", "serdes";
	
};

&cpsw9g_mdio {
	status = "okay";
	pinctrl-names = "default";
	pinctrl-0 = <&mdio0_pins_default>;
	//reset-gpios = <&exp2 17 GPIO_ACTIVE_LOW>;
	reset-post-delay-us = <120000>;
	//bus_freq = <1000000>;
	#address-cells = <1>;
	#size-cells = <0>;

	cpsw9g_phy0: ethernet-phy@4 {
		reg = <4>;
	};
	cpsw9g_phy1: ethernet-phy@5 {
		reg = <5>;
	};
	cpsw9g_phy2: ethernet-phy@8 {
		reg = <8>;
	};
	cpsw9g_phy3: ethernet-phy@10 {
		reg = <10>;
	};
	cpsw9g_phy4: ethernet-phy@12 {
	reg = <12>;
	};
	cpsw9g_phy13: ethernet-phy@13 {
    reg = <13>;
	ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
    ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
    };
};

 删除 j7-main-R5f0_0-fw   

4.删除 uenv.txt 覆层

5.  ethtool eth show link

root@j721e-evm:~# ethtool eth2
Settings for eth2:
        Supported ports: [ TP    MII ]
        Supported link modes:   1000baseT/Full
        Supported pause frame use: Symmetric
        Supports auto-negotiation: No
        Supported FEC modes: Not reported
        Advertised link modes:  Not reported
        Advertised pause frame use: Symmetric
        Advertised auto-negotiation: No
        Advertised FEC modes: Not reported
        Speed: 1000Mb/s
        Duplex: Full
        Auto-negotiation: off
        Port: Twisted Pair
        PHYAD: 13
        Transceiver: external
        MDI-X: Unknown
        Supports Wake-on: d
        Wake-on: d
        Current message level: 0x000020f7 (8439)
                               drv probe link ifdown ifup rx_err tx_err hw
        Link detected: yes
root@j721e-evm:~#
root@j721e-evm:~#

6. RGMII 链路、Ω、但无法 ping  

root@j721e-evm:/home/weston/scripts# ./j7_devmem2_cpsw9g_check_status.sh
    Platform: J7 TDA4VM
    Command:  k3conf
MDIO_ALIVE_REG (0x0c000f08) = 0x00000000
MDIO_LINK_REG (0x0c000f0c) = 0x00000000
please input your port: 1-8 3
CTRLMMR_ENET 3 CTRL (0x0010404c) = 0x00000002
        PORT_MODE_SEL          : 2h RGMII
        RGMII_ID_MODE          : 0h Internal Transmit Desaly
CPSW SS RGMII 3 STATUS (0x0c000038) = 0x0000000D
        FULLDUPLEX           : 1h Full duplex
        SPEED                : 1000Mbps
        LINK                 : 1h Link is up
CPSW_SS_STATUS_SGMII_LINK_REG (0x0c000078) = 0x00000000
        SGMII1_LINK          : 0h No
CPSW_SS_SGMII_CONTROL_REG_ 3 (0x0c000310) = 0x00000000
        TEST_PATTERN_EN      : 0h operation
        MASTER               : 0h Slave Mode
        LOOPBACK             : 0h Not in internal loopback mode
        MR_NP_LOADED         : 0h --------
        FAST_LINK_TIMER      : 0h link timer 10ms in FIBER mode and 1.6ms in SGMII mode
        MA_AN_RESTART        : 0h Write 1h and tehn 0h to this bit caused the auto negotiation
        MR_AN_ENABLE         : 0h wirte 1 to this bit enbales the auto negotiation progess
CPSW_SS_SGMII_STATUS_REG_ 3 (0x0c000314) = 0x00000028
        LOCK                  : 0h SEDES PLL isn't locked
        MR_AN_COMPLETE        : 0h no AUTO Negotiation is not complete
        AN_EEROR              : 0h no negotiation error
        LINK                  : 0h link is not up
root@j721e-evm:/home/weston/scripts#

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    您能分享看到的内核日志吗? 该定制板是或 EVM 吗? 用于端口 3 RGMII 的 phy 器件是什么?

    此致、
    Tanmay

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    phy 端使用了哪些延迟设置。 您在 MAC 侧使用内部发送延迟。 您能否确认您正在设置 Phy 侧的 Rx 延迟?

    您能共享器件树中使用的 phy 节点吗?

    此致、
    Tanmay

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:  

    我理解的与 器件树中的 phy 节点相关的内容。 仅需 k3-j721e-common-proc-board.dts (port3)  

    	rgmii3_default_pins: rgmii3-default-pins {
    	pinctrl-single,pins = <
    		J721E_IOPAD(0xb0, PIN_INPUT, 4) /* (AF28) PRG0_PRU0_GPO0.RGMII3_RD0 */
    		J721E_IOPAD(0xb4, PIN_INPUT, 4) /* (AE28) PRG0_PRU0_GPO1.RGMII3_RD1 */
    		J721E_IOPAD(0xb8, PIN_INPUT, 4) /* (AE27) PRG0_PRU0_GPO2.RGMII3_RD2 */
    		J721E_IOPAD(0xbc, PIN_INPUT, 4) /* (AD26) PRG0_PRU0_GPO3.RGMII3_RD3 */
    		J721E_IOPAD(0xc8, PIN_INPUT, 4) /* (AE26) PRG0_PRU0_GPO6.RGMII3_RXC */
    		J721E_IOPAD(0xc0, PIN_INPUT, 4) /* (AD25) PRG0_PRU0_GPO4.RGMII3_RX_CTL */
    		J721E_IOPAD(0xdc, PIN_OUTPUT, 4) /* (AJ28) PRG0_PRU0_GPO11.RGMII3_TD0 */
    		J721E_IOPAD(0xe0, PIN_OUTPUT, 4) /* (AH27) PRG0_PRU0_GPO12.RGMII3_TD1 */
    		J721E_IOPAD(0xe4, PIN_OUTPUT, 4) /* (AH29) PRG0_PRU0_GPO13.RGMII3_TD2 */
    		J721E_IOPAD(0xe8, PIN_OUTPUT, 4) /* (AG28) PRG0_PRU0_GPO14.RGMII3_TD3 */
    		J721E_IOPAD(0xf0, PIN_OUTPUT, 4) /* (AH28) PRG0_PRU0_GPO16.RGMII3_TXC */
    		J721E_IOPAD(0xec, PIN_OUTPUT, 4) /* (AG27) PRG0_PRU0_GPO15.RGMII3_TX_CTL */
    	>;
    };
    
    
    
    &cpsw0 {
    	status = "okay";
    	pinctrl-names = "default";
        pinctrl-0 = <&rgmii3_default_pins>;
    };
    &cpsw0_port1 {
    	status = "disabled";
    };
    
    &cpsw0_port2 {
    	status = "okay";
    	phy-handle = <&cpsw9g_phy0>;
    	phy-mode = "sgmii";
    	mac-address = [00 00 00 00 00 00];
    	phys = <&cpsw0_phy_gmii_sel 2>,<&serdes0_sgmii_link>;
    	//phy-names = "portmode", "serdes-phy";
    	phy-names = "portmode", "serdes";
    };
    
    &cpsw0_port3 {
    	status = "okay";
    	phy-handle = <&cpsw9g_phy13>;
    	phy-mode = "rgmii-rxid";
    	mac-address = [00 00 00 00 00 00];
    	phys = <&cpsw0_phy_gmii_sel 3>;
    };
    
    &cpsw0_port4 {
    	status = "disabled";
    };
    
    &cpsw0_port5 {
    	status = "okay";
    	phy-handle = <&cpsw9g_phy1>;
    	phy-mode = "sgmii";
    	mac-address = [00 00 00 00 00 00];
    	phys = <&cpsw0_phy_gmii_sel 5>,<&serdes4_sgmii_link>;
        // phy-names = "portmode", "serdes-phy";
    	phy-names = "portmode", "serdes";
    	 
    };
    
    &cpsw0_port6 {
    	status = "okay";
    	phy-handle = <&cpsw9g_phy2>;
    	phy-mode = "sgmii";
    	mac-address = [00 00 00 00 00 00];
    	phys = <&cpsw0_phy_gmii_sel 6>;
    	//phy-names = "portmode", "serdes-phy";
    	phy-names = "portmode", "serdes";
    	
    };
    
    &cpsw0_port7 {
    	status = "okay";
    	phy-handle = <&cpsw9g_phy3>;
    	phy-mode = "sgmii";
    	mac-address = [00 00 00 00 00 00];
    	phys = <&cpsw0_phy_gmii_sel 7>;
    	//phy-names = "portmode", "serdes-phy";
    	phy-names = "portmode", "serdes";
    	
    };
    
    &cpsw0_port8 {
    	status = "okay";
    	phy-handle = <&cpsw9g_phy4>;
    	phy-mode = "sgmii";
    	mac-address = [00 00 00 00 00 00];
    	phys = <&cpsw0_phy_gmii_sel 8>;
    	//phy-names = "portmode", "serdes-phy";
    	phy-names = "portmode", "serdes";
    	
    };
    
    &cpsw9g_mdio {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&mdio0_pins_default>;
    	//reset-gpios = <&exp2 17 GPIO_ACTIVE_LOW>;
    	reset-post-delay-us = <120000>;
    	//bus_freq = <1000000>;
    	#address-cells = <1>;
    	#size-cells = <0>;
    
    	cpsw9g_phy0: ethernet-phy@4 {
    		reg = <4>;
    	};
    	cpsw9g_phy1: ethernet-phy@5 {
    		reg = <5>;
    	};
    	cpsw9g_phy2: ethernet-phy@8 {
    		reg = <8>;
    	};
    	cpsw9g_phy3: ethernet-phy@10 {
    		reg = <10>;
    	};
    	cpsw9g_phy4: ethernet-phy@12 {
    	reg = <12>;
    	};
    	cpsw9g_phy13: ethernet-phy@13 {
        reg = <13>;
    	ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
        ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
        };
    };

     

    您能告诉我 DTS 中的其他设置、谢谢您。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    您是否可以在使用 ethool 命令运行 ping 时查看 CPSW 端口 3 统计信息?
    # ethtool -S eth2

    此外、确保 RGMII3 引脚不用于任何其他功能、通过读取 PADCONFIG 寄存器进行交叉确认。

    此致、
    Sudheer