请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
大家好、TI 伙计们、
我也有同样的问题。
icssg0、icssg1 net 端口在 v09.02.01.09 时工作正常、但升级到 v11.01.05.03(我是 v11 k3-am642-evm.dts)、它们都不正确、即使没有在“IP link show“列表中。
引导日志:
[ 12.161093] davinci_mdio 30032400.mdio: Configuring MDIO in manual mode [ 12.265489] davinci_mdio 30032400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 12.424706] davinci_mdio 30032400.mdio: phy[1]: device 30032400.mdio:01, driver Micrel KSZ9031 Gigabit PHY [ 12.434567] davinci_mdio 30032400.mdio: phy[4]: device 30032400.mdio:04, driver Micrel KSZ9031 Gigabit PHY [ 12.834682] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:03] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL) [ 12.888498] davinci_mdio 300b2400.mdio: Configuring MDIO in manual mode [ 12.898292] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ 12.983929] davinci_mdio 300b2400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 13.038809] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@a4000000 [ 13.070134] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:07] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL) [ 13.116966] k3-m4-rproc 5000000.m4fss: configured M4F for remoteproc mode [ 13.149298] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode [ 13.228482] davinci_mdio 300b2400.mdio: phy[2]: device 300b2400.mdio:02, driver Micrel KSZ9031 Gigabit PHY [ 13.331629] remoteproc remoteproc0: 5000000.m4fss is available [ 13.471404] m_can_platform 20701000.can: m_can device registered (irq=521, version=32) [ 13.491896] m_can_platform 20711000.can: m_can device registered (irq=522, version=32) [ 13.517262] k3_r5_rproc bus@f4000:r5fss@78000000: MCU cluster requires both R5F cores to be enabled but num_cores is set to = 1 [ 13.540883] k3_r5_rproc bus@f4000:r5fss@78400000: MCU cluster requires both R5F cores to be enabled but num_cores is set to = 1 [ 13.620589] remoteproc remoteproc0: powering up 5000000.m4fss [ 13.626727] remoteproc remoteproc0: Booting fw image am64-mcu-m4f0_0-fw, size 88248 [ 13.638496] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node m4f-dma-memory@a4000000 [ 13.648989] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd [ 13.656693] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [ 13.664271] virtio_rpmsg_bus virtio0: rpmsg host is online [ 13.670174] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7) [ 13.677137] remoteproc remoteproc0: remote processor 5000000.m4fss is now up [ 13.979553] remoteproc remoteproc1: 3000a000.txpru is available [ 13.991307] remoteproc remoteproc2: 3000c000.txpru is available [ 14.017734] remoteproc remoteproc3: 3008a000.txpru is available [ 14.061833] remoteproc remoteproc4: 3008c000.txpru is available [ 14.393555] remoteproc remoteproc5: 30034000.pru is available [ 14.421173] remoteproc remoteproc6: 30084000.rtu is available [ 14.438435] remoteproc remoteproc7: 30038000.pru is available [ 14.465648] remoteproc remoteproc8: 30006000.rtu is available [ 14.486233] remoteproc remoteproc9: 30004000.rtu is available [ 14.506094] remoteproc remoteproc10: 300b8000.pru is available [ 14.526243] remoteproc remoteproc11: 30086000.rtu is available [ 14.557108] remoteproc remoteproc12: 300b4000.pru is available [ 14.728936] icssg-prueth icssg0-eth: error -ENODEV: iep0 get failed [ 14.755175] icssg-prueth icssg1-eth: error -ENODEV: iep0 get failed [ 14.808784] m_can_platform 20701000.can main_mcan0: renamed from can0 [ 14.930864] m_can_platform 20711000.can main_mcan1: renamed from can1
此致、
Wei