This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 关于:AM6442:使用 AM6442 的 ICSSG0 和 ICSSG1 内核

Guru**** 2556220 points
Other Parts Discussed in Thread: AM6442

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1568704/re-am6442-using-icssg0-and-icssg1-core-of-am6442



大家好、TI 伙计们、

我也有同样的问题。  

icssg0、icssg1 net 端口在 v09.02.01.09 时工作正常、但升级到 v11.01.05.03(我是 v11 k3-am642-evm.dts)、它们都不正确、即使没有在“IP link show“列表中。

引导日志:

[   12.161093] davinci_mdio 30032400.mdio: Configuring MDIO in manual mode
[   12.265489] davinci_mdio 30032400.mdio: davinci mdio revision 1.7, bus freq 1000000
[   12.424706] davinci_mdio 30032400.mdio: phy[1]: device 30032400.mdio:01, driver Micrel KSZ9031 Gigabit PHY
[   12.434567] davinci_mdio 30032400.mdio: phy[4]: device 30032400.mdio:04, driver Micrel KSZ9031 Gigabit PHY
[   12.834682] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:03] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[   12.888498] davinci_mdio 300b2400.mdio: Configuring MDIO in manual mode
[   12.898292] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[   12.983929] davinci_mdio 300b2400.mdio: davinci mdio revision 1.7, bus freq 1000000
[   13.038809] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@a4000000
[   13.070134] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:07] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[   13.116966] k3-m4-rproc 5000000.m4fss: configured M4F for remoteproc mode
[   13.149298] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
[   13.228482] davinci_mdio 300b2400.mdio: phy[2]: device 300b2400.mdio:02, driver Micrel KSZ9031 Gigabit PHY
[   13.331629] remoteproc remoteproc0: 5000000.m4fss is available
[   13.471404] m_can_platform 20701000.can: m_can device registered (irq=521, version=32)
[   13.491896] m_can_platform 20711000.can: m_can device registered (irq=522, version=32)
[   13.517262] k3_r5_rproc bus@f4000:r5fss@78000000: MCU cluster requires both R5F cores to be enabled but num_cores is set to = 1
[   13.540883] k3_r5_rproc bus@f4000:r5fss@78400000: MCU cluster requires both R5F cores to be enabled but num_cores is set to = 1
[   13.620589] remoteproc remoteproc0: powering up 5000000.m4fss
[   13.626727] remoteproc remoteproc0: Booting fw image am64-mcu-m4f0_0-fw, size 88248
[   13.638496] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node m4f-dma-memory@a4000000
[   13.648989] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[   13.656693] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[   13.664271] virtio_rpmsg_bus virtio0: rpmsg host is online
[   13.670174] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7)
[   13.677137] remoteproc remoteproc0: remote processor 5000000.m4fss is now up
[   13.979553] remoteproc remoteproc1: 3000a000.txpru is available
[   13.991307] remoteproc remoteproc2: 3000c000.txpru is available
[   14.017734] remoteproc remoteproc3: 3008a000.txpru is available
[   14.061833] remoteproc remoteproc4: 3008c000.txpru is available
[   14.393555] remoteproc remoteproc5: 30034000.pru is available
[   14.421173] remoteproc remoteproc6: 30084000.rtu is available
[   14.438435] remoteproc remoteproc7: 30038000.pru is available
[   14.465648] remoteproc remoteproc8: 30006000.rtu is available
[   14.486233] remoteproc remoteproc9: 30004000.rtu is available
[   14.506094] remoteproc remoteproc10: 300b8000.pru is available
[   14.526243] remoteproc remoteproc11: 30086000.rtu is available
[   14.557108] remoteproc remoteproc12: 300b4000.pru is available
[   14.728936] icssg-prueth icssg0-eth: error -ENODEV: iep0 get failed
[   14.755175] icssg-prueth icssg1-eth: error -ENODEV: iep0 get failed
[   14.808784] m_can_platform 20701000.can main_mcan0: renamed from can0
[   14.930864] m_can_platform 20711000.can main_mcan1: renamed from can1

此致、

Wei

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     大家好、TI 伙计们、

    我将相同的 dts 复制到 uboot、所有 icssg net 端口都正常工作。

    此致、

    Wei

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    对于未来的读者,Wei 最初将此作为对现有线程  AM6442 的响应:使用 AM6442 的 ICSSG0 和 ICSSG1 核心。 我已经把他的问题移到了一个单独的主题。

    您好、Wei、

    您是否说在更新 uboot DTS 后 SDK 11.1 按预期工作? 或者、您在这里仍然需要帮助?

    此致、

    Nick  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    不、我已经 解决了。

    此致、

    Wei