器件型号: AM62L
HII、
根据 TI_Thread DDR 优化更改、我完成了所有操作。
但经过以下日志后电路板无法引导:
NOTICE: bl1_plat_arch_setup arch setup
NOTICE: Booting Trusted Firmware
NOTICE: BL1: v2.12.0(release):11.00.15-dirty
NOTICE: BL1: Built : 12:24:23, May 29 2025
NOTICE: BL1: dram_class: 11
NOTICE: lpddr4: post start - PI training status=0x27c0a000
NOTICE: bl1_platform_setup DDR init done
NOTICE: k3_bl1_handoff ENTERING WFI - end of bl1
NOTICE: BL31: v2.12.0(release):11.00.15-dirty
NOTICE: BL31: Built : 12:24:23, May 29 2025
NOTICE: SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.12-v11.00.12 (Fancy Rat)')
ERROR: Agent 0 Protocol 0x10 Message 0x7: not supportedU-Boot SPL 2025.01-00464-g1d6ba4a32cdd-dirty (May 29 2025 - 19:36:32 +0000)
如果我缺少任何必要的更改、请指导我吗?
此致、
参数