This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] J721S2XSOMXEVM:构建 C7X MMALIB 示例

Guru**** 2756805 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1615485/j721s2xsomxevm-build-c7x-mmalib-example

器件型号: J721S2XSOMXEVM

您好:

我尝试使用以下命令使用指南为 C7X 构建 mmalib 示例:

make -j12 TARGET_CPU=C7120 LINK_LIBS=1 cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX TEST_CASE=13 TEST_ENV=EVM CHECKPARAMS=1 SOC=J7ES TARGET_BUILD=release

但我得到了这个错误:  

[C7X] Compiling C MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.c
[C7X] Compiling C MMALIB_CNN_convolve_row_ixX_ixX_oxX_idat.c
Copying Prebuilt binary /home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/ti/mmalib/concerto/c7120/lnk.cmd to /home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/lnk.cmd
"/home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/ti/mmalib/src/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.c", line 849: warning #1219-D: arithmetic on pointer to void or function type
"/home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/ti/mmalib/src/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.c", line 850: warning #1219-D: arithmetic on pointer to void or function type
"/home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/ti/mmalib/src/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.c", line 887: warning #1219-D: arithmetic on pointer to void or function type
"/home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/ti/mmalib/src/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.c", line 888: warning #1219-D: arithmetic on pointer to void or function type
Linking /home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX_C7120.out
<Linking>
"/home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/lnk.cmd", line 99: warning #19014-D:
   undefined preprocessor symbol 'j784s4'
"/home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/lnk.cmd", line 131: warning #19014-D:
   undefined preprocessor symbol 'j784s4'

 undefined                                              first referenced                                                                                                                                         
  symbol                                                    in file                                                                                                                                              
 ---------                                              ----------------                                                                                                                                         
 MMA_CNNLIB_convolveBiasReLUCompute_ixX_ixX_oxX_perfEst /home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/module/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.obj
 ddr_size                                               /home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/module/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.obj
 msmc_size                                              /home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/module/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX/MMALIB_CNN_convolve_row_ixX_ixX_oxX_d.obj

error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking;
   "/home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02
   _00_06/out/C7120/release/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX_C712
   0.out" not built

>> Compilation failure
make: [concerto/finale.mak:134: /home/amohame8/ti/ti-processor-sdk-rtos-j721s2-evm-11_02_00_06/mmalib_11_02_00_06/out/C7120/release/cnn_c7xmma/MMALIB_CNN_convolve_row_ixX_ixX_oxX_C7120.out] Error 1 (ignored)

 

RTOS SDK:11_02_00_06

MMALIB:11_02_00_06

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、
    我能够使用以下命令成功构建。 请尝试同样的方法。


    此致、
    Ben Eapen Thomas