请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AM4376 您好!
我想在 AM4376的 ADC0块上感测测试设置的模拟信号。
模拟信号的范围为0V 至5V。 AM4376的 ADC0/ ADC1的电源电压(VDDA)为1.8V。
有人能不能建议我如何实现这一点???
谢谢你。
Dhara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.