This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Linux
我正在关注 wiki 以构建 Arago 图像。 我在最后几天去了一次痛苦的调整工具的过程
而是推特问题、但我到达了一个无法通过的步骤。
|/usr/bin/ld:/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/llvm-3.6.build/Release/lib/libLLVMARMCodeGen.a (ARMISelLging.o):`.rodata._ZL20getExtensionTo64BitsRKN4lvm3EVTE'段中偏移量0x100的错误重新定位符号索引(0x40000120 >= 0x627)
|/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/llvm-3.6.build/Release/lib/libLLVMARMCodeGen.a (ARMISelLing.o):添加符号时出错:错误值
| collect2:错误:LD 返回1退出状态
|/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/git/Makefile.rules:1199:目标'/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/llvm-3.6.build/Release/lib/libLLVM-3.6.so 的配方失败
|制造[1]:***[/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/llvm-3.6.build/Release/lib/libLLVM-3.6.so ]错误1.
| make[1]:离开目录'/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/llvm-3.6.build/tools/llvm-shlib
|/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/git/Makefile.rules:873:目标"全部"配方失败
|制造:***[全部]错误1.
|错误:OE_runmake 失败
|错误:函数失败:DO 编译(日志文件位于/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-llvm3.6-native/3.6-r5/temp/log.do_compile.6627)
错误:任务6478 (虚拟:本机:/home/marius/APPS/BOARDS/TI/SDK_Processor/tisdk/sources/meta-arago/meta-arago-extras/recipes-core/llvm/ti-llvm3.6_3.6.bb、DO 编译)失败、退出代码为"1"
谢谢你。