This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] Linux/TCA8418E:适用于 linux3.14及以上版本的 GPIO 驱动程序

Guru**** 2588495 points
Other Parts Discussed in Thread: TCA8418

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/592584/linux-tca8418e-gpio-driver-for-linux3-14-and-up

器件型号:TCA8418E
主题中讨论的其他器件:TCA8418

工具/软件:Linux

大家好

我将 TCA8418用作 I.MX6电路板上的 GPIO 按钮。如何配置它。与 adp5588不兼容? 我的 Linux 版本为3.14和4.1.15