请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TCA8418E 主题中讨论的其他器件:TCA8418
工具/软件:Linux
大家好
我将 TCA8418用作 I.MX6电路板上的 GPIO 按钮。如何配置它。与 adp5588不兼容? 我的 Linux 版本为3.14和4.1.15
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.