This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] Linux:发出"Continuous Tx"在蓝牙中? 射频性能测量

Guru**** 2589300 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/589299/linux-command-issue-of-continuous-tx-in-bluetooth-rf-performance-measurement

Thread 中讨论的其他器件:WL1837

工具/软件:Linux

硬件:omap4470 + wl1837

软件:Android4.1.2 (4AJ.2.2_OMAP4_Jelly_Bean Release_Notes)

维客: processors.wiki.ti.com/.../WL18xx_Bluetopia_PM_Bluetooth_RF_Testing

我想测试 wl1837蓝牙? 射频性能测量、例如 TX/RX 等。我使用 hcitool 配置 wl1837 BT、执行"continuous TX"命令后、信号在2个扇区内消失。

测试模式:
hool citcmd 0x06 0x03
hcitool cmd 0x03 0x05 0x02 0x00 0x03
hool citcmd 0x03 0x1a 0x03

连续 TX:
hcitool cmd 0x3f 0x01fb 0x01 0xff 0x00 0x00 0x00 0x01
hcitool cmd 0x3f 0x01ca 0x62 0x09 0x01 0x00 0x07 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00