This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320DM8165:DM8165能否使用 H264编码器同时对2个1080p60流进行实时编码?

Guru**** 2589300 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/634029/tms320dm8165-can-dm8165-encode-2-1080p60-streams-with-h264-encoder-simultaneously-in-real-time

器件型号:TMS320DM8165
Thread 中讨论的其他器件:DM385

尊敬的:

 DM8165具有2个 hdvicps、随着我们的控制、每个 hdvicp 都可以使用 H264编码器实时编码1个1080p60流。
 目前、我们需要输入2个1080p60数据流、并同时使用 H264编码器(实时)对二者进行编码。


 1) 1) DM8165能否满足要求?  
 2) 2) DDR 带宽满足要求?  
 3)或任何其他组件不符合要求?  

谢谢!

王淑 o