Other Parts Discussed in Thread: AM3359
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AM3359 我们建议连接需要2.5V 电压 的 MARVELL GigPHY (RGMII)、而 AM3359指示 VDDSHV5为1.8V/3.3V。
它们是否兼容?
还是可以将2.5V 电源扩展到 控制器 RGMII (1)的 VDDSHV5?
建议!
系统
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.