请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:OMAP-L138 各位专家、您好!
让我确认"6.19.2 UART 电气数据/时序"。
下表列出了"最小值:U - 2"和"最大值:U + 2"、"2"的单位是否以 ns 为单位? 还是%?
当波特率为9600时、我询问2ns 对于104.1[us]是否过于严格。
此致、
还不错
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.